sl_wfx_context_t Struct Reference

Structure used to maintain the Wi-Fi solution context on the host side.

Data Fields

uint8_t event_payload_buffer [512]
Event payload associated with the last posted event.
uint8_t firmware_build
Firmware build version.
uint8_t firmware_minor
Firmware minor version.
uint8_t firmware_major
Firmware major version.
uint16_t data_frame_id
Frame ID incremented by sl_wfx_send_ethernet_frame .
uint16_t used_buffers
Number of buffers currently in use by the WFx chip.
uint8_t wfx_opn [14]
OPN of the part.
sl_wfx_mac_address_t mac_addr_0
Mac address used by WFx interface 0, station.
sl_wfx_mac_address_t mac_addr_1
Mac address used by WFx interface 1, softap.
sl_wfx_state_t state
State of the WFx Wi-Fi chip.

Structure used to maintain the Wi-Fi solution context on the host side.

Definition at line 397 of file sl_wfx_constants.h .

Field Documentation

◆ data_frame_id

uint16_t sl_wfx_context_t::data_frame_id

Frame ID incremented by sl_wfx_send_ethernet_frame .

Definition at line 402 of file sl_wfx_constants.h .

Referenced by sl_wfx_send_ethernet_frame() .

◆ event_payload_buffer

uint8_t sl_wfx_context_t::event_payload_buffer[512]

Event payload associated with the last posted event.

Definition at line 398 of file sl_wfx_constants.h .

◆ firmware_build

uint8_t sl_wfx_context_t::firmware_build

Firmware build version.

Definition at line 399 of file sl_wfx_constants.h .

◆ firmware_major

uint8_t sl_wfx_context_t::firmware_major

Firmware major version.

Definition at line 401 of file sl_wfx_constants.h .

◆ firmware_minor

uint8_t sl_wfx_context_t::firmware_minor

Firmware minor version.

Definition at line 400 of file sl_wfx_constants.h .

◆ mac_addr_0

sl_wfx_mac_address_t sl_wfx_context_t::mac_addr_0

Mac address used by WFx interface 0, station.

Definition at line 405 of file sl_wfx_constants.h .

Referenced by sl_wfx_set_mac_address() .

◆ mac_addr_1

sl_wfx_mac_address_t sl_wfx_context_t::mac_addr_1

Mac address used by WFx interface 1, softap.

Definition at line 406 of file sl_wfx_constants.h .

Referenced by sl_wfx_set_mac_address() .

◆ state

sl_wfx_state_t sl_wfx_context_t::state

State of the WFx Wi-Fi chip.

Definition at line 407 of file sl_wfx_constants.h .

Referenced by sl_wfx_disable_device_power_save() , and sl_wfx_enable_device_power_save() .

◆ used_buffers

uint16_t sl_wfx_context_t::used_buffers

Number of buffers currently in use by the WFx chip.

Definition at line 403 of file sl_wfx_constants.h .

Referenced by sl_wfx_send_request() .

◆ wfx_opn

uint8_t sl_wfx_context_t::wfx_opn[14]

OPN of the part.

Definition at line 404 of file sl_wfx_constants.h .

Referenced by sl_wfx_get_opn() .


The documentation for this struct was generated from the following file:
  • sl_wfx_constants.h