EM35x standalone bootloader public definitions.
Required Custom Functions | |
void | bootloaderMenu (void) |
This function must be implemented, providing a bootloader menu. |
Available Bootloader Library Functions | |
Functions implemented by the bootloader library that may be used by custom functions. | |
BL_Status | receiveImage (uint8_t commState) |
Puts the bootloader into a mode where it will receive an image. commState indicates whether the image is received via serial (COMM_SERIAL) or over the air (COMM_RADIO) | |
bool | checkDebugMenuOption (uint8_t ch) |
A hook to the bootloader library for it to check for extra menu options. Only used for ember internal debug builds, not normally needed. | |
BL_Status | initOtaState (void) |
Initialize OTA Bootloader state. | |
BL_Status | checkOtaStart (void) |
Check to see if the bootloader has detected an OTA upload start. | |
BL_Status | receiveOtaImage (void) |
Puts the bootloader into a mode where it will receive an image over the air. The function checkOtaStart() should have been called first and it should have returned with a status of BL_SUCCESS before calling this function. | |
bool | paIsPresent (void) |
Uses the information in the PHY_CONFIG token to determine if a power amplifier is present in the node design. | |
bool | halCheckIntegrity (void) |
Validate application integrity by running AES-MMO hash and comparing to AAT. |
Detailed Description
EM35x standalone bootloader public definitions.
See standalone-bootloader.h
for source code.
Function Documentation
void bootloaderMenu | ( | void |
| ) |
This function must be implemented, providing a bootloader menu.
bool checkDebugMenuOption | ( | uint8_t | ch | ) |
A hook to the bootloader library for it to check for extra menu options. Only used for ember internal debug builds, not normally needed.
- Returns
- true if the option was handled, false if not.
BL_Status checkOtaStart | ( | void |
| ) |
Check to see if the bootloader has detected an OTA upload start.
- Note
- OTA support hooks are subject to change!
- Returns
- BL_Status of the success of the function.
bool halCheckIntegrity | ( | void |
| ) |
Validate application integrity by running AES-MMO hash and comparing to AAT.
- Returns
- false if fails integrity check, true if pass
BL_Status initOtaState | ( | void |
| ) |
Initialize OTA Bootloader state.
- Note
- OTA support hooks are subject to change!
- Returns
- BL_Status of the success of the function.
bool paIsPresent | ( | void |
| ) |
Uses the information in the PHY_CONFIG token to determine if a power amplifier is present in the node design.
- Note
- This function must not be called before emBootloaderRadioBoot().
- Returns
- true if a power amplifier is present, false otherwise.
BL_Status receiveImage | ( | uint8_t | commState | ) |
Puts the bootloader into a mode where it will receive an image. commState indicates whether the image is received via serial (COMM_SERIAL) or over the air (COMM_RADIO)
BL_Status receiveOtaImage | ( | void |
| ) |
Puts the bootloader into a mode where it will receive an image over the air. The function checkOtaStart() should have been called first and it should have returned with a status of BL_SUCCESS before calling this function.
- Note
- OTA support hooks are subject to change!
- Returns
- BL_Status of the success of the function.