Compiler and Platform specific definitions and typedefs common to all platforms.
|
#define | MEMSET(d, v, l) memset(d, v, l) |
| Friendly convenience macro pointing to the C Stdlib functions.
|
|
#define | MEMCOPY(d, s, l) memcpy(d, s, l) |
|
#define | MEMMOVE(d, s, l) memmove(d, s, l) |
|
#define | MEMPGMCOPY(d, s, l) memcpy(d, s, l) |
|
#define | MEMCOMPARE(s0, s1, l) memcmp(s0, s1, l) |
|
#define | MEMPGMCOMPARE(s0, s1, l) memcmp(s0, s1, l) |
|
#define | TRUE 1 |
| An alias for one, used for clarity.
|
|
#define | FALSE 0 |
| An alias for zero, used for clarity.
|
|
#define | NULL ((void *)0) |
| The null pointer.
|
|
#define | BIT(x) (1U << (x)) |
| Useful to reference a single bit of a byte.
|
|
#define | BIT32(x) (((uint32_t) 1) << (x)) |
| Useful to reference a single bit of an uint32_t type.
|
|
#define | SETBIT(reg, bit) (reg) |= BIT(bit) |
| Sets bit in the reg register or byte.
|
|
#define | SETBITS(reg, bits) (reg) |= (bits) |
| Sets the bits in the reg register or the byte as specified in the bitmask bits .
|
|
#define | CLEARBIT(reg, bit) (reg) &= ~(BIT(bit)) |
| Clears a bit in the reg register or byte.
|
|
#define | CLEARBITS(reg, bits) (reg) &= ~(bits) |
| Clears the bits in the reg register or byte as specified in the bitmask bits .
|
|
#define | READBIT(reg, bit) ((reg) & (BIT(bit))) |
| Returns the value of bit within the register or byte reg .
|
|
#define | READBITS(reg, bits) ((reg) & (bits)) |
| Returns the value of the bitmask bits within the register or byte reg .
|
|
#define | LOW_BYTE(n) ((uint8_t)((n) & 0xFF)) |
| Returns the low byte of the 16-bit value n as an uint8_t .
|
|
#define | HIGH_BYTE(n) ((uint8_t)(LOW_BYTE((n) >> 8))) |
| Returns the high byte of the 16-bit value n as an uint8_t .
|
|
#define | HIGH_LOW_TO_INT(high, low) |
| Returns the value built from the two uint8_t values high and low .
|
|
#define | INT8U_TO_INT32U(byte3, byte2, byte1, byte0) |
| Returns the value built from the four uint8_t as an uint32_t .
|
|
#define | BYTE_0(n) ((uint8_t)((n) & 0xFF)) |
| Returns the low byte of the 32-bit value n as an uint8_t .
|
|
#define | BYTE_1(n) BYTE_0((n) >> 8) |
| Returns the second byte of the 32-bit value n as an uint8_t .
|
|
#define | BYTE_2(n) BYTE_0((n) >> 16) |
| Returns the third byte of the 32-bit value n as an uint8_t .
|
|
#define | BYTE_3(n) BYTE_0((n) >> 24) |
| Returns the high byte of the 32-bit value n as an uint8_t .
|
|
#define | BYTE_4(n) BYTE_0((n) >> 32) |
| Returns the fifth byte of the 64-bit value n as an uint8_t .
|
|
#define | BYTE_5(n) BYTE_0((n) >> 40) |
| Returns the sixth byte of the 64-bit value n as an uint8_t .
|
|
#define | BYTE_6(n) BYTE_0((n) >> 48) |
| Returns the seventh byte of the 64-bit value n as an uint8_t .
|
|
#define | BYTE_7(n) BYTE_0((n) >> 56) |
| Returns the high byte of the 64-bit value n as an uint8_t .
|
|
#define | COUNTOF(a) (sizeof(a) / sizeof(a[0])) |
| Returns the number of entries in an array.
|
|
#define | elapsedTimeInt8u(oldTime, newTime) ((uint8_t) ((uint8_t)(newTime) - (uint8_t)(oldTime))) |
| Returns the elapsed time between two 8 bit values. Result may not be valid if the time samples differ by more than 127.
|
|
#define | elapsedTimeInt16u(oldTime, newTime) ((uint16_t) ((uint16_t)(newTime) - (uint16_t)(oldTime))) |
| Returns the elapsed time between two 16 bit values. Result may not be valid if the time samples differ by more than 32767.
|
|
#define | elapsedTimeInt32u(oldTime, newTime) ((uint32_t) ((uint32_t)(newTime) - (uint32_t)(oldTime))) |
| Returns the elapsed time between two 32 bit values. Result may not be valid if the time samples differ by more than 2147483647.
|
|
#define | MAX_INT8U_VALUE (0xFF) |
| Returns true if t1 is greater than t2. Can only account for 1 wrap around of the variable before it is wrong.
|
|
#define | HALF_MAX_INT8U_VALUE (0x80) |
| Returns the elapsed time between two 8 bit values. Result may not be valid if the time samples differ by more than 127.
|
|
#define | timeGTorEqualInt8u(t1, t2) (elapsedTimeInt8u(t2, t1) <= (HALF_MAX_INT8U_VALUE)) |
| Returns the elapsed time between two 8 bit values. Result may not be valid if the time samples differ by more than 127.
|
|
#define | MAX_INT16U_VALUE (0xFFFF) |
| Returns true if t1 is greater than t2. Can only account for 1 wrap around of the variable before it is wrong.
|
|
#define | HALF_MAX_INT16U_VALUE (0x8000) |
| Returns the elapsed time between two 8 bit values. Result may not be valid if the time samples differ by more than 127.
|
|
#define | timeGTorEqualInt16u(t1, t2) (elapsedTimeInt16u(t2, t1) <= (HALF_MAX_INT16U_VALUE)) |
| Returns the elapsed time between two 8 bit values. Result may not be valid if the time samples differ by more than 127.
|
|
#define | MAX_INT32U_VALUE (0xFFFFFFFFUL) |
| Returns true if t1 is greater than t2. Can only account for 1 wrap around of the variable before it is wrong.
|
|
#define | HALF_MAX_INT32U_VALUE (0x80000000UL) |
| Returns the elapsed time between two 8 bit values. Result may not be valid if the time samples differ by more than 127.
|
|
#define | timeGTorEqualInt32u(t1, t2) (elapsedTimeInt32u(t2, t1) <= (HALF_MAX_INT32U_VALUE)) |
| Returns the elapsed time between two 8 bit values. Result may not be valid if the time samples differ by more than 127.
|
|
#define | UNUSED_VAR(x) (void)(x) |
|
#define | DEBUG_LEVEL BASIC_DEBUG |
| Set debug level based on whether DEBUG or DEBUG_STRIPPED are defined.
|
|
#define | STATIC_ASSERT(__condition, __errorstr) |
| Disable static assertions on compilers that don't support them.
|
Compiler and Platform specific definitions and typedefs common to all platforms.
platform-common.h
provides PLATFORM_HEADER defaults and common definitions. This head should never be included directly, it should only be included by the specific PLATFORM_HEADER used by your platform.
See platform-common.h
for source code.
#define BIT |
( |
|
x | ) |
(1U << (x)) |
Useful to reference a single bit of a byte.
#define BIT32 |
( |
|
x | ) |
(((uint32_t) 1) << (x)) |
Useful to reference a single bit of an uint32_t type.
#define BYTE_0 |
( |
|
n | ) |
((uint8_t)((n) & 0xFF)) |
Returns the low byte of the 32-bit value n
as an uint8_t
.
#define BYTE_1 |
( |
|
n | ) |
BYTE_0((n) >> 8) |
Returns the second byte of the 32-bit value n
as an uint8_t
.
#define BYTE_2 |
( |
|
n | ) |
BYTE_0((n) >> 16) |
Returns the third byte of the 32-bit value n
as an uint8_t
.
#define BYTE_3 |
( |
|
n | ) |
BYTE_0((n) >> 24) |
Returns the high byte of the 32-bit value n
as an uint8_t
.
#define BYTE_4 |
( |
|
n | ) |
BYTE_0((n) >> 32) |
Returns the fifth byte of the 64-bit value n
as an uint8_t
.
#define BYTE_5 |
( |
|
n | ) |
BYTE_0((n) >> 40) |
Returns the sixth byte of the 64-bit value n
as an uint8_t
.
#define BYTE_6 |
( |
|
n | ) |
BYTE_0((n) >> 48) |
Returns the seventh byte of the 64-bit value n
as an uint8_t
.
#define BYTE_7 |
( |
|
n | ) |
BYTE_0((n) >> 56) |
Returns the high byte of the 64-bit value n
as an uint8_t
.
#define CLEARBIT |
( |
|
reg, |
|
|
|
bit |
|
) |
| (reg) &= ~(BIT(bit)) |
Clears a bit in the reg
register or byte.
- Note
- Assuming
reg
is an IO register, some platforms (such as the AVR) can implement this in a single atomic operation.
#define CLEARBITS |
( |
|
reg, |
|
|
|
bits |
|
) |
| (reg) &= ~(bits) |
Clears the bits in the reg
register or byte as specified in the bitmask bits
.
- Note
- This is never a single atomic operation.
#define COUNTOF |
( |
|
a | ) |
(sizeof(a) / sizeof(a[0])) |
Returns the number of entries in an array.
Set debug level based on whether DEBUG or DEBUG_STRIPPED are defined.
#define elapsedTimeInt16u |
( |
|
oldTime, |
|
|
|
newTime |
|
) |
| ((uint16_t) ((uint16_t)(newTime) - (uint16_t)(oldTime))) |
Returns the elapsed time between two 16 bit values. Result may not be valid if the time samples differ by more than 32767.
#define elapsedTimeInt32u |
( |
|
oldTime, |
|
|
|
newTime |
|
) |
| ((uint32_t) ((uint32_t)(newTime) - (uint32_t)(oldTime))) |
Returns the elapsed time between two 32 bit values. Result may not be valid if the time samples differ by more than 2147483647.
#define elapsedTimeInt8u |
( |
|
oldTime, |
|
|
|
newTime |
|
) |
| ((uint8_t) ((uint8_t)(newTime) - (uint8_t)(oldTime))) |
Returns the elapsed time between two 8 bit values. Result may not be valid if the time samples differ by more than 127.
An alias for zero, used for clarity.
#define HALF_MAX_INT16U_VALUE (0x8000) |
Returns the elapsed time between two 8 bit values. Result may not be valid if the time samples differ by more than 127.
#define HALF_MAX_INT32U_VALUE (0x80000000UL) |
Returns the elapsed time between two 8 bit values. Result may not be valid if the time samples differ by more than 127.
#define HALF_MAX_INT8U_VALUE (0x80) |
Returns the elapsed time between two 8 bit values. Result may not be valid if the time samples differ by more than 127.
#define HIGH_BYTE |
( |
|
n | ) |
((uint8_t)(LOW_BYTE((n) >> 8))) |
Returns the high byte of the 16-bit value n
as an uint8_t
.
#define HIGH_LOW_TO_INT |
( |
|
high, |
|
|
|
low |
|
) |
| |
Value:( \
((uint16_t) (((uint16_t) (high)) << 8)) \
+ ((uint16_t) ((low) & 0xFF)) \
)
Returns the value built from the two uint8_t
values high
and low
.
#define INT8U_TO_INT32U |
( |
|
byte3, |
|
|
|
byte2, |
|
|
|
byte1, |
|
|
|
byte0 |
|
) |
| |
Value:( \
(((uint32_t) (byte3)) << 24) \
+ (((uint32_t) (byte2)) << 16) \
+ (((uint32_t) (byte1)) << 8) \
+ ((uint32_t) ((byte0) & 0xFF)) \
)
Returns the value built from the four uint8_t
as an uint32_t
.
#define LOW_BYTE |
( |
|
n | ) |
((uint8_t)((n) & 0xFF)) |
Returns the low byte of the 16-bit value n
as an uint8_t
.
#define MAX_INT16U_VALUE (0xFFFF) |
Returns true if t1 is greater than t2. Can only account for 1 wrap around of the variable before it is wrong.
#define MAX_INT32U_VALUE (0xFFFFFFFFUL) |
Returns true if t1 is greater than t2. Can only account for 1 wrap around of the variable before it is wrong.
#define MAX_INT8U_VALUE (0xFF) |
Returns true if t1 is greater than t2. Can only account for 1 wrap around of the variable before it is wrong.
#define MEMCOMPARE |
( |
|
s0, |
|
|
|
s1, |
|
|
|
l |
|
) |
| memcmp(s0, s1, l) |
#define MEMCOPY |
( |
|
d, |
|
|
|
s, |
|
|
|
l |
|
) |
| memcpy(d, s, l) |
#define MEMMOVE |
( |
|
d, |
|
|
|
s, |
|
|
|
l |
|
) |
| memmove(d, s, l) |
#define MEMPGMCOMPARE |
( |
|
s0, |
|
|
|
s1, |
|
|
|
l |
|
) |
| memcmp(s0, s1, l) |
#define MEMPGMCOPY |
( |
|
d, |
|
|
|
s, |
|
|
|
l |
|
) |
| memcpy(d, s, l) |
#define MEMSET |
( |
|
d, |
|
|
|
v, |
|
|
|
l |
|
) |
| memset(d, v, l) |
Friendly convenience macro pointing to the C Stdlib functions.
#define READBIT |
( |
|
reg, |
|
|
|
bit |
|
) |
| ((reg) & (BIT(bit))) |
Returns the value of bit
within the register or byte reg
.
#define READBITS |
( |
|
reg, |
|
|
|
bits |
|
) |
| ((reg) & (bits)) |
Returns the value of the bitmask bits
within the register or byte reg
.
#define SETBIT |
( |
|
reg, |
|
|
|
bit |
|
) |
| (reg) |= BIT(bit) |
Sets bit
in the reg
register or byte.
- Note
- Assuming
reg
is an IO register, some platforms (such as the AVR) can implement this in a single atomic operation.
#define SETBITS |
( |
|
reg, |
|
|
|
bits |
|
) |
| (reg) |= (bits) |
Sets the bits in the reg
register or the byte as specified in the bitmask bits
.
- Note
- This is never a single atomic operation.
#define STATIC_ASSERT |
( |
|
__condition, |
|
|
|
__errorstr |
|
) |
| |
Disable static assertions on compilers that don't support them.
Returns the elapsed time between two 8 bit values. Result may not be valid if the time samples differ by more than 127.
Returns the elapsed time between two 8 bit values. Result may not be valid if the time samples differ by more than 127.
Returns the elapsed time between two 8 bit values. Result may not be valid if the time samples differ by more than 127.
An alias for one, used for clarity.
#define UNUSED_VAR |
( |
|
x | ) |
(void)(x) |
Useful macro for avoiding compiler warnings related to unused function arguments or unused variables.