EmberMultiPhyRadioParameters Struct Reference
Holds radio parameters.
#include <
ember-types.h
>
Data Fields | |
int8_t | radioTxPower |
uint8_t | radioPage |
uint8_t | radioChannel |
Holds radio parameters.
This is mainly useful for dual PHY and switched radio device (2.4 Ghz or SubGhz) to retrieve radio parameters.
Field Documentation
uint8_t EmberMultiPhyRadioParameters::radioChannel |
uint8_t EmberMultiPhyRadioParameters::radioPage |
int8_t EmberMultiPhyRadioParameters::radioTxPower |
The documentation for this struct was generated from the following file:
ember-types.h