EmberChildData Struct Reference
This structure contains information about child nodes.
#include <
ember-types.h
>
Data Fields | |
EmberEUI64 | eui64 |
EmberNodeType | type |
EmberNodeId | id |
uint8_t | phy |
uint8_t | power |
uint8_t | timeout |
This structure contains information about child nodes.
Field Documentation
EmberEUI64 EmberChildData::eui64 |
EmberNodeId EmberChildData::id |
uint8_t EmberChildData::phy |
uint8_t EmberChildData::power |
uint8_t EmberChildData::timeout |
EmberNodeType EmberChildData::type |
The documentation for this struct was generated from the following file:
ember-types.h