EmberZllNetwork Struct Reference
Information about the ZLL network and specific device that responded to a ZLL scan request.
#include <
zll-types.h
>
Data Fields | |
EmberZigbeeNetwork | zigbeeNetwork |
EmberZllSecurityAlgorithmData | securityAlgorithm |
EmberEUI64 | eui64 |
EmberNodeId | nodeId |
EmberZllState | state |
EmberNodeType | nodeType |
uint8_t | numberSubDevices |
uint8_t | totalGroupIdentifiers |
uint8_t | rssiCorrection |
Information about the ZLL network and specific device that responded to a ZLL scan request.
Field Documentation
EmberEUI64 EmberZllNetwork::eui64 |
EmberNodeId EmberZllNetwork::nodeId |
EmberNodeType EmberZllNetwork::nodeType |
uint8_t EmberZllNetwork::numberSubDevices |
uint8_t EmberZllNetwork::rssiCorrection |
EmberZllSecurityAlgorithmData EmberZllNetwork::securityAlgorithm |
EmberZllState EmberZllNetwork::state |
uint8_t EmberZllNetwork::totalGroupIdentifiers |
EmberZigbeeNetwork EmberZllNetwork::zigbeeNetwork |
The documentation for this struct was generated from the following file:
zll-types.h