EmberZigbeeNetwork Struct Reference
Defines a ZigBee network and the associated parameters.
#include <
ember-types.h
>
Data Fields | |
uint16_t | panId |
uint8_t | channel |
bool | allowingJoin |
uint8_t | extendedPanId [EXTENDED_PAN_ID_SIZE] |
uint8_t | stackProfile |
uint8_t | nwkUpdateId |
Defines a ZigBee network and the associated parameters.
Field Documentation
bool EmberZigbeeNetwork::allowingJoin |
uint8_t EmberZigbeeNetwork::channel |
uint8_t EmberZigbeeNetwork::extendedPanId[EXTENDED_PAN_ID_SIZE] |
uint8_t EmberZigbeeNetwork::nwkUpdateId |
uint16_t EmberZigbeeNetwork::panId |
uint8_t EmberZigbeeNetwork::stackProfile |
The documentation for this struct was generated from the following file:
ember-types.h