Packet Buffers
Macros | |
#define | LOG_PACKET_BUFFER_SIZE 5 |
Buffers hold 32 bytes. Defined as the log to ensure it is a power of 2. | |
#define | PACKET_BUFFER_SIZE (1 << LOG_PACKET_BUFFER_SIZE) |
Buffers hold 32 bytes. | |
#define | EMBER_NULL_MESSAGE_BUFFER 0xFF |
Provides the message buffer equivalent of NULL. | |
#define | emberMessageBufferLength(buffer) (emMessageBufferLengths[buffer]) |
Returns the length of a buffer. Implemented as a macro for improved efficiency. |
Functions | |
uint8_t * | emberMessageBufferContents (EmberMessageBuffer buffer) |
Gets a pointer to a buffer's contents. This pointer can be used to access only the first PACKET_BUFFER_SIZE bytes in the buffer. To read a message composed of multiple buffers, use emberCopyFromLinkedBuffers(). | |
void | emberSetMessageBufferLength (EmberMessageBuffer buffer, uint8_t newLength) |
Sets the length of a buffer. | |
void | emberHoldMessageBuffer (EmberMessageBuffer buffer) |
Holds a message buffer by incrementing its reference count. Implemented as a macro for improved efficiency. | |
void | emberReleaseMessageBuffer (EmberMessageBuffer buffer) |
Releases a message buffer by decrementing its reference count. Implemented as a macro for improved efficiency. | |
uint8_t | emberPacketBufferFreeCount (void) |
Retrieves the current number of free packet buffers. |
Buffer Functions | |
EmberMessageBuffer | emberAllocateLinkedBuffers (uint8_t count) |
Allocates one or more linked buffers. | |
EmberMessageBuffer | emberFillStackBuffer (unsigned int count,...) |
Allocates a stack buffer and fills the buffer with data passed in the function call. | |
#define | emberStackBufferLink(buffer) (emPacketBufferLinks[(buffer)]) |
Returns the buffer that follows this one in the message. EMBER_NULL_MESSAGE_BUFFER is returned if there is no following buffer. | |
#define | emberSetStackBufferLink(buffer, newLink) (emPacketBufferLinks[(buffer)] = (newLink)) |
Sets the buffer following this one in the message. The final buffer in the message has EMBER_NULL_MESSAGE_BUFFER as its link. | |
#define | emberAllocateStackBuffer() (emberAllocateLinkedBuffers(1)) |
Allocates a stack buffer. |
Linked Buffer Utilities | |
The plural "buffers" in the names of these procedures is a reminder that they deal with linked chains of buffers. | |
EmberMessageBuffer | emberFillLinkedBuffers (uint8_t *contents, uint8_t length) |
Allocates a chain of stack buffers sufficient to hold length bytes of data and fills the buffers with the data in contents. If the value of contents is NULL, the buffers are allocated but not filled. | |
void | emberCopyToLinkedBuffers (const uint8_t *contents, EmberMessageBuffer buffer, uint8_t startIndex, uint8_t length) |
Copies a specified number of bytes of data into a buffer, starting at a specified index in the buffer array. Buffer links are followed as required. No buffers are allocated or released. | |
void | emberCopyFromLinkedBuffers (EmberMessageBuffer buffer, uint8_t startIndex, uint8_t *contents, uint8_t length) |
Copies length bytes of data from a buffer to contents , starting at a specified index in the buffer array. Buffer links are followed as required. | |
void | emberCopyBufferBytes (EmberMessageBuffer to, uint16_t toIndex, EmberMessageBuffer from, uint16_t fromIndex, uint16_t count) |
Copies a specified number of bytes of data from one buffer into another. Buffer links are followed as required. No buffers are allocated or released. | |
void | emberMoveBufferBytes (EmberMessageBuffer to, uint16_t toIndex, EmberMessageBuffer from, uint16_t fromIndex, uint16_t count) |
Allocates a chain of stack buffers sufficient to hold length bytes of data and fills the buffers with the data in contents. If the value of contents is NULL, the buffers are allocated but not filled. | |
EmberStatus | emberAppendToLinkedBuffers (EmberMessageBuffer buffer, uint8_t *contents, uint8_t length) |
Appends length bytes from contents onto a buffer. Combines the functionality of ::setPacketBuffersLength() and ::copyToPacketBuffers(). | |
EmberStatus | emberAppendPgmStringToLinkedBuffers (EmberMessageBuffer buffer, const char *suffix) |
Appends a string from program space (flash) to a buffer. | |
EmberStatus | emberSetLinkedBuffersLength (EmberMessageBuffer buffer, uint8_t length) |
Sets the length of a chain of buffers, adding or removing trailing buffers as needed. | |
uint8_t * | emberGetLinkedBuffersPointer (EmberMessageBuffer buffer, uint8_t index) |
Gets a pointer to a specified byte in a linked list of buffers. | |
uint8_t | emberGetLinkedBuffersByte (EmberMessageBuffer buffer, uint8_t index) |
Gets a specified byte in a linked list of buffers. | |
void | emberSetLinkedBuffersByte (EmberMessageBuffer buffer, uint8_t index, uint8_t byte) |
Sets the indexed byte in a linked list of buffers. | |
uint16_t | emberGetLinkedBuffersLowHighInt16u (EmberMessageBuffer buffer, uint8_t index) |
Gets a little-endian 2-byte value from a linked list of buffers. | |
void | emberSetLinkedBuffersLowHighInt16u (EmberMessageBuffer buffer, uint8_t index, uint16_t value) |
Sets a little-endian 2-byte value in a linked list of buffers. | |
uint32_t | emberGetLinkedBuffersLowHighInt32u (EmberMessageBuffer buffer, uint8_t index) |
Gets a little-endian 4-byte value from a linked list of buffers. | |
void | emberSetLinkedBuffersLowHighInt32u (EmberMessageBuffer buffer, uint8_t index, uint32_t value) |
Sets a little-endian 4-byte value in a linked list of buffers. | |
EmberMessageBuffer | emberCopyLinkedBuffers (EmberMessageBuffer buffer) |
Copies a chain of linked buffers. | |
EmberMessageBuffer | emberMakeUnsharedLinkedBuffer (EmberMessageBuffer buffer, bool isShared) |
Creates a new, unshared copy of a specified buffer, if that buffer is shared. If it isn't shared, increments the reference count by 1 so that the user of the returned buffer can release it in either case. |
Detailed Description
These functions implement a fixed-block-size memory management scheme to store and manipulate EmberZNet packets. Buffers are identified to clients with a 1-byte ID.
Buffers can be linked together to create longer packets. The utility procedures allow you to treat a linked chain of buffers as a single buffer.
Freeing a buffer automatically decrements the reference count of any following buffer, possibly freeing the following buffer as well.
Packet buffers may be allocated, held, and released.
See packet-buffer.h
for source code.
Macro Definition Documentation
#define EMBER_NULL_MESSAGE_BUFFER 0xFF |
Provides the message buffer equivalent of NULL.
#define emberAllocateStackBuffer | ( |
| ) | (emberAllocateLinkedBuffers(1)) |
Allocates a stack buffer.
- Returns
- A newly allocated buffer, or EMBER_NULL_MESSAGE_BUFFER if no buffer is available.
#define emberMessageBufferLength | ( | buffer | ) | (emMessageBufferLengths[buffer]) |
Returns the length of a buffer. Implemented as a macro for improved efficiency.
- Parameters
-
buffer
A buffer.
- Returns
- The buffer length.
#define emberSetStackBufferLink | ( | buffer, |
|
newLink |
|||
) | (emPacketBufferLinks[(buffer)] = (newLink)) |
Sets the buffer following this one in the message. The final buffer in the message has EMBER_NULL_MESSAGE_BUFFER as its link.
- Parameters
-
buffer
The buffer whose link is to be set. newLink
The buffer that is to follow buffer
.
#define emberStackBufferLink | ( | buffer | ) | (emPacketBufferLinks[(buffer)]) |
Returns the buffer that follows this one in the message. EMBER_NULL_MESSAGE_BUFFER is returned if there is no following buffer.
- Parameters
-
buffer
The buffer whose following buffer is desired.
- Returns
- Returns the buffer that follows
buffer
in the message. EMBER_NULL_MESSAGE_BUFFER is returned if there is no following buffer.
#define LOG_PACKET_BUFFER_SIZE 5 |
Buffers hold 32 bytes. Defined as the log to ensure it is a power of 2.
#define PACKET_BUFFER_SIZE (1 << LOG_PACKET_BUFFER_SIZE) |
Buffers hold 32 bytes.
Function Documentation
EmberMessageBuffer emberAllocateLinkedBuffers | ( | uint8_t | count | ) |
Allocates one or more linked buffers.
- Parameters
-
count
The number of buffers to allocate.
- Returns
- The first buffer in the newly allocated chain of buffers, or EMBER_NULL_MESSAGE_BUFFER if insufficient buffers are available.
EmberStatus emberAppendPgmStringToLinkedBuffers | ( | EmberMessageBuffer | buffer, |
const char * | suffix |
||
) |
Appends a string from program space (flash) to a buffer.
- Parameters
-
buffer
The buffer to append data to. suffix
The string in program space to append.
- Returns
- EMBER_SUCCESS if sufficient buffers are available, and EMBER_NO_BUFFERS if not.
EmberStatus emberAppendToLinkedBuffers | ( | EmberMessageBuffer | buffer, |
uint8_t * | contents, |
||
uint8_t | length |
||
) |
Appends length
bytes from contents
onto a buffer. Combines the functionality of ::setPacketBuffersLength() and ::copyToPacketBuffers().
- Parameters
-
buffer
The buffer to append data to. contents
A pointer to data to append. length
The number of bytes of data to append.
- Returns
- EMBER_SUCCESS if sufficient buffers are available, and EMBER_NO_BUFFERS if not.
void emberCopyBufferBytes | ( | EmberMessageBuffer | to, |
uint16_t | toIndex, |
||
EmberMessageBuffer | from, |
||
uint16_t | fromIndex, |
||
uint16_t | count |
||
) |
Copies a specified number of bytes of data from one buffer into another. Buffer links are followed as required. No buffers are allocated or released.
- Parameters
-
to
The buffer to copy data into. toIndex
The position in the destination buffer at which copying should start. from
The buffer to copy data from. fromIndex
The position in the source buffer at which copying should start. count
The number of bytes of data to copy.
void emberCopyFromLinkedBuffers | ( | EmberMessageBuffer | buffer, |
uint8_t | startIndex, |
||
uint8_t * | contents, |
||
uint8_t | length |
||
) |
Copies length
bytes of data from a buffer to contents
, starting at a specified index in the buffer array. Buffer links are followed as required.
- Parameters
-
buffer
The buffer to copy data from. startIndex
The buffer index at which copying should start. contents
A pointer to data to copy from the buffer. length
The number of bytes of data to copy.
EmberMessageBuffer emberCopyLinkedBuffers | ( | EmberMessageBuffer | buffer | ) |
Copies a chain of linked buffers.
- Parameters
-
buffer
The first buffer in the chain to copy.
- Returns
- A newly created copy of the
buffer
chain.
void emberCopyToLinkedBuffers | ( | const uint8_t * | contents, |
EmberMessageBuffer | buffer, |
||
uint8_t | startIndex, |
||
uint8_t | length |
||
) |
Copies a specified number of bytes of data into a buffer, starting at a specified index in the buffer array. Buffer links are followed as required. No buffers are allocated or released.
- Parameters
-
contents
A pointer to data to copy into the buffer. buffer
The buffer to copy data into. startIndex
The buffer index at which copying should start. length
The number of bytes of data to copy.
EmberMessageBuffer emberFillLinkedBuffers | ( | uint8_t * | contents, |
uint8_t | length |
||
) |
Allocates a chain of stack buffers sufficient to hold length
bytes of data and fills the buffers with the data in contents. If the value of contents is NULL, the buffers are allocated but not filled.
- Parameters
-
contents
A pointer to data to place in the allocated buffers. length
The buffer length.
- Returns
- The first buffer in a series of linked stack buffers, or EMBER_NULL_MESSAGE_BUFFER if insufficient buffers are available.
EmberMessageBuffer emberFillStackBuffer | ( | unsigned int | count, |
... |
|||
) |
Allocates a stack buffer and fills the buffer with data passed in the function call.
- Parameters
-
count
The buffer length. ...
count
bytes, which will be placed in the buffer.
- Returns
- A newly allocated buffer, or EMBER_NULL_MESSAGE_BUFFER if no buffer is available.
uint8_t emberGetLinkedBuffersByte | ( | EmberMessageBuffer | buffer, |
uint8_t | index |
||
) |
Gets a specified byte in a linked list of buffers.
- Parameters
-
buffer
The buffer that the requested byte must come from. index
The index of the requested byte.
- Returns
- A byte.
uint16_t emberGetLinkedBuffersLowHighInt16u | ( | EmberMessageBuffer | buffer, |
uint8_t | index |
||
) |
Gets a little-endian 2-byte value from a linked list of buffers.
- Parameters
-
buffer
The buffer containing the 2-byte value. index
The index of the low byte.
- Returns
- The 2-byte value.
uint32_t emberGetLinkedBuffersLowHighInt32u | ( | EmberMessageBuffer | buffer, |
uint8_t | index |
||
) |
Gets a little-endian 4-byte value from a linked list of buffers.
- Parameters
-
buffer
The buffer containing the 4-byte value. index
The index of the low byte.
- Returns
- The 4-byte value.
uint8_t* emberGetLinkedBuffersPointer | ( | EmberMessageBuffer | buffer, |
uint8_t | index |
||
) |
Gets a pointer to a specified byte in a linked list of buffers.
- Parameters
-
buffer
The buffer that the requested byte must come from. index
The index of the requested byte.
- Returns
- A pointer to the requested byte.
void emberHoldMessageBuffer | ( | EmberMessageBuffer | buffer | ) |
Holds a message buffer by incrementing its reference count. Implemented as a macro for improved efficiency.
- Parameters
-
buffer
A buffer.
EmberMessageBuffer emberMakeUnsharedLinkedBuffer | ( | EmberMessageBuffer | buffer, |
bool | isShared |
||
) |
Creates a new, unshared copy of a specified buffer, if that buffer is shared. If it isn't shared, increments the reference count by 1 so that the user of the returned buffer can release it in either case.
- Parameters
-
buffer
The buffer to copy. isShared
A flag indicating whether the buffer is shared.
- Returns
- A fresh copy of
buffer
ifisShared
is true, andbuffer
ifisShared
is not true.
uint8_t* emberMessageBufferContents | ( | EmberMessageBuffer | buffer | ) |
Gets a pointer to a buffer's contents. This pointer can be used to access only the first PACKET_BUFFER_SIZE bytes in the buffer. To read a message composed of multiple buffers, use emberCopyFromLinkedBuffers().
- Parameters
-
buffer
The buffer whose contents are desired.
- Returns
- Returns a pointer to the contents of
buffer
.
void emberMoveBufferBytes | ( | EmberMessageBuffer | to, |
uint16_t | toIndex, |
||
EmberMessageBuffer | from, |
||
uint16_t | fromIndex, |
||
uint16_t | count |
||
) |
Allocates a chain of stack buffers sufficient to hold length
bytes of data and fills the buffers with the data in contents. If the value of contents is NULL, the buffers are allocated but not filled.
- Parameters
-
contents
A pointer to data to place in the allocated buffers. length
The buffer length.
- Returns
- The first buffer in a series of linked stack buffers, or EMBER_NULL_MESSAGE_BUFFER if insufficient buffers are available.
uint8_t emberPacketBufferFreeCount | ( | void |
| ) |
Retrieves the current number of free packet buffers.
- Returns
- The number of free packet buffers.
void emberReleaseMessageBuffer | ( | EmberMessageBuffer | buffer | ) |
Releases a message buffer by decrementing its reference count. Implemented as a macro for improved efficiency.
- Parameters
-
buffer
A buffer.
void emberSetLinkedBuffersByte | ( | EmberMessageBuffer | buffer, |
uint8_t | index, |
||
uint8_t | byte |
||
) |
Sets the indexed byte in a linked list of buffers.
- Parameters
-
buffer
The buffer holding the byte to be set. index
The index of the byte to set. byte
The value to set the byte to.
EmberStatus emberSetLinkedBuffersLength | ( | EmberMessageBuffer | buffer, |
uint8_t | length |
||
) |
Sets the length of a chain of buffers, adding or removing trailing buffers as needed.
- Parameters
-
buffer
The buffer whose length is to be set. length
The length to set.
- Returns
- EMBER_SUCCESS if changing
buffer's
length bylength
bytes does not require additional buffers or if sufficient buffers are available, and EMBER_NO_BUFFERS if not.
void emberSetLinkedBuffersLowHighInt16u | ( | EmberMessageBuffer | buffer, |
uint8_t | index, |
||
uint16_t | value |
||
) |
Sets a little-endian 2-byte value in a linked list of buffers.
- Parameters
-
buffer
The buffer to set the 2-byte value in. index
The index of the low byte. value
The 2-byte value to set.
void emberSetLinkedBuffersLowHighInt32u | ( | EmberMessageBuffer | buffer, |
uint8_t | index, |
||
uint32_t | value |
||
) |
Sets a little-endian 4-byte value in a linked list of buffers.
- Parameters
-
buffer
The buffer to set the 2-byte value in. index
The index of the low byte. value
The 4-byte value to set.
void emberSetMessageBufferLength | ( | EmberMessageBuffer | buffer, |
uint8_t | newLength |
||
) |
Sets the length of a buffer.
When asserts are enabled, attempting to set a length greater than the size of the buffer triggers an assert.
- Parameters
-
buffer
A buffer newLength
The length to set the buffer to.