|
EmberStatus | emberNodeDescriptorRequest (EmberNodeId target, EmberApsOption options) |
| Request the specified node to send its node descriptor. The node descriptor contains information about the capabilities of the ZigBee node. It describes logical type, APS flags, frequency band, MAC capabilities flags, manufacturer code and maximum buffer size. It is defined in the ZigBee Application Framework Specification.
|
|
EmberStatus | emberPowerDescriptorRequest (EmberNodeId target, EmberApsOption options) |
| Request the specified node to send its power descriptor. The power descriptor gives a dynamic indication of the power status of the node. It describes current power mode, available power sources, current power source and current power source level. It is defined in the ZigBee Application Framework Specification.
|
|
EmberStatus | emberSimpleDescriptorRequest (EmberNodeId target, uint8_t targetEndpoint, EmberApsOption options) |
| Request the specified node to send the simple descriptor for the specified endpoint. The simple descriptor contains information specific to a single endpoint. It describes the application profile identifier, application device identifier, application device version, application flags, application input clusters and application output clusters. It is defined in the ZigBee Application Framework Specification.
|
|
EmberStatus | emberActiveEndpointsRequest (EmberNodeId target, EmberApsOption options) |
| Request the specified node to send a list of its active endpoints. An active endpoint is one for which a simple descriptor is available.
|
|
EmberStatus | emberBindRequest (EmberNodeId target, EmberEUI64 source, uint8_t sourceEndpoint, uint16_t clusterId, uint8_t type, EmberEUI64 destination, EmberMulticastId groupAddress, uint8_t destinationEndpoint, EmberApsOption options) |
| Send a request to create a binding entry with the specified contents on the specified node.
|
|
EmberStatus | emberUnbindRequest (EmberNodeId target, EmberEUI64 source, uint8_t sourceEndpoint, uint16_t clusterId, uint8_t type, EmberEUI64 destination, EmberMulticastId groupAddress, uint8_t destinationEndpoint, EmberApsOption options) |
| Send a request to remove a binding entry with the specified contents from the specified node.
|
|
EmberStatus | emberLqiTableRequest (EmberNodeId target, uint8_t startIndex, EmberApsOption options) |
| Request the specified node to send its LQI (neighbor) table. The response gives PAN ID, EUI64, node ID and cost for each neighbor. The EUI64 is only available if security is enabled. The other fields in the response are set to zero. The response format is defined in the ZigBee Device Profile Specification.
|
|
EmberStatus | emberRoutingTableRequest (EmberNodeId target, uint8_t startIndex, EmberApsOption options) |
| Request the specified node to send its routing table. The response gives destination node ID, status and many-to-one flags, and the next hop node ID. The response format is defined in the ZigBee Device Profile Specification.
|
|
EmberStatus | emberBindingTableRequest (EmberNodeId target, uint8_t startIndex, EmberApsOption options) |
| Request the specified node to send its nonvolatile bindings. The response gives source address, source endpoint, cluster ID, destination address and destination endpoint for each binding entry. The response format is defined in the ZigBee Device Profile Specification. Note that bindings that have the Ember-specific UNICAST_MANY_TO_ONE_BINDING type are reported as having the standard UNICAST_BINDING type.
|
|
EmberStatus | emberLeaveRequest (EmberNodeId target, EmberEUI64 deviceAddress, uint8_t leaveRequestFlags, EmberApsOption options) |
| Request the specified node to remove the specified device from the network. The device to be removed must be the node to which the request is sent or one of its children.
|
|
EmberStatus | emberPermitJoiningRequest (EmberNodeId target, uint8_t duration, uint8_t authentication, EmberApsOption options) |
| Request the specified node to allow or disallow association.
|
|
void | emberSetZigDevRequestRadius (uint8_t radius) |
| Change the default radius for broadcast ZDO requests.
|
|
uint8_t | emberGetZigDevRequestRadius (void) |
| Retrieve the default radius for broadcast ZDO requests.
|
|
uint8_t | emberGetLastZigDevRequestSequence (void) |
| Provide access to the application ZDO transaction sequence number for last request. This function has been deprecated and replaced by emberGetLastAppZigDevRequestSequence().
|
|
uint8_t | emberGetLastAppZigDevRequestSequence (void) |
| Provide access to the application ZDO transaction sequence number for last request.
|
|
EmberStatus | ezspEndDeviceBindRequest (EmberNodeId localNodeId, EmberEUI64 localEui64, uint8_t endpoint, uint16_t profile, uint8_t inCount, uint8_t outCount, uint16_t *inClusters, uint16_t *outClusters, EmberApsOption options) |
| An end device bind request to the coordinator. If the coordinator receives a second end device bind request then a binding is created for every matching cluster.
|
For getting information about nodes of a ZigBee network via a ZigBee Device Object (ZDO). See zigbee-device-library.h
and zigbee-device-common.h
for source code.
The ZDO library provides functions that construct and send several common ZDO requests. It also provides a function for extracting the two addresses from a ZDO address response. The format of all the ZDO requests and responses that the stack supports is described in stack/include/zigbee-device-stack.h
. Since the library doesn't handle all of these requests and responses, the application must construct any other requests it wishes to send and decode any other responses it wishes to receive.
The request sending functions do the following:
- Construct a correctly formatted payload buffer.
- Fill in the APS frame with the correct values.
- Send the message by calling either emberSendBroadcast() or emberSendUnicast().
The result of the send is reported to the application as normal via emberMessageSentHandler().
The following code shows an example of an application's use of emberSimpleDescriptorRequest(). The command interpreter would call this function and supply the arguments.
void sendSimpleDescriptorRequest(EmberCommandState *state)
{
targetEndpoint,
emberSerialPrintf(SERIAL_PORT, "emberSimpleDescriptorRequest failed\r\n");
}
}
The following code shows an example of an application's use of emberDecodeAddressResponse().
{
{
break;
}
default:
}
} else {
}
}
For getting information about nodes of a ZigBee network via a ZigBee Device Object (ZDO). See zigbee-device-host.h
and zigbee-device-common.h
for source code.
The ZDO library provides functions that construct and send several common ZDO requests. It also provides a function for extracting the two addresses from a ZDO address response. The format of all the ZDO requests and responses that the stack supports is described in stack/include/zigbee-device-stack.h
. Since the library doesn't handle all of these requests and responses, the application must construct any other requests it wishes to send and decode any other responses it wishes to receive.
The request sending functions do the following:
- Construct a correctly formatted payload buffer.
- Fill in the APS frame with the correct values.
- Send the message by calling either ::ezspSendBroadcast() or ::ezspSendUnicast().
The result of the send is reported to the application as normal via ::ezspMessageSentHandler().
The following code shows an example of an application's use of emberSimpleDescriptorRequest(). The command interpreter would call this function and supply the arguments.
void sendSimpleDescriptorRequest(EmberCommandState *state)
{
targetEndpoint,
emberSerialPrintf(SERIAL_PORT, "emberSimpleDescriptorRequest failed\r\n");
}
}
The following code shows an example of an application's use of ezspDecodeAddressResponse().
uint8_t lastHopLqi,
int8_t lastHopRssi,
uint8_t bindingIndex,
uint8_t addressIndex,
uint8_t messageLength,
uint8_t *messageContents)
{
{
eui64);
break;
}
default:
}
} else {
}
}
#define ZDO_MESSAGE_OVERHEAD 1 |
ZDO messages start with a sequence number.
Request the specified node to send its nonvolatile bindings. The response gives source address, source endpoint, cluster ID, destination address and destination endpoint for each binding entry. The response format is defined in the ZigBee Device Profile Specification. Note that bindings that have the Ember-specific UNICAST_MANY_TO_ONE_BINDING type are reported as having the standard UNICAST_BINDING type.
- Parameters
-
target | The node whose binding table is desired. |
startIndex | The index of the first binding entry to include in the response. |
options | The options to use when sending the request. See emberSendUnicast() for a description. |
- Returns
- An EmberStatus value. EMBER_SUCCESS, EMBER_NO_BUFFERS, EMBER_NETWORK_DOWN or EMBER_NETWORK_BUSY.
Extracts the EUI64 and the node ID from an address response message.
- Parameters
-
- Returns
- Returns the node ID from the response if the response status was EMBER_ZDP_SUCCESS. Otherwise, returns EMBER_NULL_NODE_ID.
An end device bind request to the coordinator. The simple descriptor of the specified endpoint is used to construct the request. If the coordinator receives a second end device bind request then a binding is created for every matching cluster.
- Parameters
-
endpoint | The endpoint on the local device whose simple descriptor will be used to create the request. |
options | The options to use when sending the request. See emberSendUnicast() for a description. |
- Returns
- An EmberStatus value. EMBER_SUCCESS, EMBER_NO_BUFFERS, EMBER_NETWORK_DOWN or EMBER_NETWORK_BUSY.
uint8_t emberGetLastAppZigDevRequestSequence |
( |
void |
| ) |
|
Provide access to the application ZDO transaction sequence number for last request.
- Returns
- Last application ZDO transaction sequence number used
uint8_t emberGetLastZigDevRequestSequence |
( |
void |
| ) |
|
Provide access to the application ZDO transaction sequence number for last request. This function has been deprecated and replaced by emberGetLastAppZigDevRequestSequence().
- Returns
- Last application ZDO transaction sequence number used
uint8_t emberGetZigDevRequestRadius |
( |
void |
| ) |
|
Retrieve the default radius for broadcast ZDO requests.
- Returns
- The radius to be used for future ZDO request broadcasts.
Request the EUI64 of a node whose 16 bit network address is known.
- Parameters
-
target | The network address of the node. |
reportKids | true to request that the target list their children in the response. |
childStartIndex | The index of the first child to list in the response. Ignored if reportKids is false. |
options | The options to use when sending the request. See emberSendUnicast() for a description. |
- Returns
- An
EmberStatus
value.
Request the specified node to remove the specified device from the network. The device to be removed must be the node to which the request is sent or one of its children.
- Parameters
-
target | The node which will remove the device. |
deviceAddress | All zeros if the target is to remove itself from the network or the EUI64 of a child of the target device to remove that child. |
leaveRequestFlags | A bitmask of leave options. Include LEAVE_REQUEST_REMOVE_CHILDREN_FLAG if the target is to remove their children and/or LEAVE_REQUEST_REJOIN_FLAG if the target is to rejoin the network immediately after leaving. |
options | The options to use when sending the request. See emberSendUnicast() for a description. |
- Returns
- An EmberStatus value. EMBER_SUCCESS, EMBER_NO_BUFFERS, EMBER_NETWORK_DOWN or EMBER_NETWORK_BUSY.
Request the specified node to send its LQI (neighbor) table. The response gives PAN ID, EUI64, node ID and cost for each neighbor. The EUI64 is only available if security is enabled. The other fields in the response are set to zero. The response format is defined in the ZigBee Device Profile Specification.
- Parameters
-
target | The node whose LQI table is desired. |
startIndex | The index of the first neighbor to include in the response. |
options | The options to use when sending the request. See emberSendUnicast() for a description. |
- Returns
- An EmberStatus value. EMBER_SUCCESS, EMBER_NO_BUFFERS, EMBER_NETWORK_DOWN or EMBER_NETWORK_BUSY.
Request the specified node to send a list of its endpoints that match the specified application profile and, optionally, lists of input and/or output clusters.
- Parameters
-
target | The node whose matching endpoints are desired. The request can be sent unicast or broadcast ONLY to the "RX-on-when-idle-address" (0xFFFD) If sent as a broadcast, any node that has matching endpoints will send a response. |
profile | The application profile to match. |
inClusters | The list of input clusters. To not match any input clusters, use EMBER_NULL_MESSAGE_BUFFER. |
outClusters | The list of output clusters. To not match any output clusters, use EMBER_NULL_MESSAGE_BUFFER. |
options | The options to use when sending the unicast request. See emberSendUnicast() for a description. This parameter is ignored if the target is a broadcast address. |
- Returns
- An EmberStatus value. EMBER_SUCCESS, EMBER_NO_BUFFERS, EMBER_NETWORK_DOWN or EMBER_NETWORK_BUSY.
Request the 16 bit network address of a node whose EUI64 is known.
- Parameters
-
target | The EUI64 of the node. |
reportKids | true to request that the target list their children in the response. |
childStartIndex | The index of the first child to list in the response. Ignored if reportKids is false. |
- Returns
- An
EmberStatus
value.
Request the specified node to send its node descriptor. The node descriptor contains information about the capabilities of the ZigBee node. It describes logical type, APS flags, frequency band, MAC capabilities flags, manufacturer code and maximum buffer size. It is defined in the ZigBee Application Framework Specification.
- Parameters
-
target | The node whose node descriptor is desired. |
options | The options to use when sending the request. See emberSendUnicast() for a description. |
- Returns
- An
EmberStatus
value. EMBER_SUCCESS, EMBER_NO_BUFFERS, EMBER_NETWORK_DOWN or EMBER_NETWORK_BUSY.
Request the specified node to allow or disallow association.
- Parameters
-
target | The node which will allow or disallow association. The request can be broadcast by using a broadcast address (0xFFFC/0xFFFD/0xFFFF). No response is sent if the request is broadcast. |
duration | A value of 0x00 disables joining. A value of 0xFF enables joining. Any other value enables joining for that number of seconds. |
authentication | Controls Trust Center authentication behavior. |
options | The options to use when sending the request. See emberSendUnicast() for a description. This parameter is ignored if the target is a broadcast address. |
- Returns
- An EmberStatus value. EMBER_SUCCESS, EMBER_NO_BUFFERS, EMBER_NETWORK_DOWN or EMBER_NETWORK_BUSY.
Request the specified node to send its power descriptor. The power descriptor gives a dynamic indication of the power status of the node. It describes current power mode, available power sources, current power source and current power source level. It is defined in the ZigBee Application Framework Specification.
- Parameters
-
target | The node whose power descriptor is desired. |
options | The options to use when sending the request. See emberSendUnicast() for a description. |
- Returns
- An EmberStatus value. EMBER_SUCCESS, EMBER_NO_BUFFERS, EMBER_NETWORK_DOWN or EMBER_NETWORK_BUSY.
Request the specified node to send its routing table. The response gives destination node ID, status and many-to-one flags, and the next hop node ID. The response format is defined in the ZigBee Device Profile Specification.
- Parameters
-
target | The node whose routing table is desired. |
startIndex | The index of the first route entry to include in the response. |
options | The options to use when sending the request. See emberSendUnicast() for a description. |
- Returns
- An EmberStatus value. EMBER_SUCCESS, EMBER_NO_BUFFERS, EMBER_NETWORK_DOWN or EMBER_NETWORK_BUSY.
void emberSetZigDevRequestRadius |
( |
uint8_t |
radius | ) |
|
Change the default radius for broadcast ZDO requests.
- Parameters
-
radius | The radius to be used for future ZDO request broadcasts. |
Request the specified node to send the simple descriptor for the specified endpoint. The simple descriptor contains information specific to a single endpoint. It describes the application profile identifier, application device identifier, application device version, application flags, application input clusters and application output clusters. It is defined in the ZigBee Application Framework Specification.
- Parameters
-
target | The node of interest. |
targetEndpoint | The endpoint on the target node whose simple descriptor is desired. |
options | The options to use when sending the request. See emberSendUnicast() for a description. |
- Returns
- An EmberStatus value. EMBER_SUCCESS, EMBER_NO_BUFFERS, EMBER_NETWORK_DOWN or EMBER_NETWORK_BUSY.
Send a request to remove a binding entry with the specified contents from the specified node.
- Parameters
-
- Returns
- An
EmberStatus
value.
Extracts the EUI64 and the node ID from an address response message.
- Parameters
-
response | The received ZDO message with cluster ID NETWORK_ADDRESS_RESPONSE or IEEE_ADDRESS_RESPONSE. |
eui64Return | The EUI64 from the response is copied here. |
- Returns
- Returns the node ID from the response if the response status was EMBER_ZDP_SUCCESS. Otherwise, returns EMBER_NULL_NODE_ID.
An end device bind request to the coordinator. If the coordinator receives a second end device bind request then a binding is created for every matching cluster.
- Parameters
-
localNodeId | The node ID of the local device. |
localEui64 | The EUI64 of the local device. |
endpoint | The endpoint to be bound. |
profile | The application profile of the endpoint. |
inCount | The number of input clusters. |
outCount | The number of output clusters. |
inClusters | The list of input clusters. |
outClusters | The list of output clusters. |
options | The options to use when sending the request. See emberSendUnicast() for a description. |
- Returns
- An EmberStatus value. EMBER_SUCCESS, EMBER_NO_BUFFERS, EMBER_NETWORK_DOWN or EMBER_NETWORK_BUSY.
EmberStatus ezspMatchDescriptorsRequest |
( |
EmberNodeId |
target, |
|
|
uint16_t |
profile, |
|
|
uint8_t |
inCount, |
|
|
uint8_t |
outCount, |
|
|
uint16_t * |
inClusters, |
|
|
uint16_t * |
outClusters, |
|
|
EmberApsOption |
options |
|
) |
| |
Request the specified node to send a list of its endpoints that match the specified application profile and, optionally, lists of input and/or output clusters.
- Parameters
-
target | The node whose matching endpoints are desired. The request can be sent unicast or broadcast ONLY to the "RX-on-when-idle-address" (0xFFFD) If sent as a broadcast, any node that has matching endpoints will send a response. |
profile | The application profile to match. |
inCount | The number of input clusters. To not match any input clusters, set this value to 0. |
outCount | The number of output clusters. To not match any output clusters, set this value to 0. |
inClusters | The list of input clusters. |
outClusters | The list of output clusters. |
options | The options to use when sending the unicast request. See emberSendUnicast() for a description. This parameter is ignored if the target is a broadcast address. |
- Returns
- An EmberStatus value. EMBER_SUCCESS, EMBER_NO_BUFFERS, EMBER_NETWORK_DOWN or EMBER_NETWORK_BUSY.