InterPanHeader Struct Reference
A struct for keeping track of all of the header info.
#include <
ami-inter-pan.h
>
Data Fields | |
uint8_t | messageType |
uint16_t | panId |
bool | hasLongAddress |
EmberNodeId | shortAddress |
EmberEUI64 | longAddress |
uint16_t | profileId |
uint16_t | clusterId |
uint16_t | groupId |
A struct for keeping track of all of the header info.
A struct for keeping track of all of the interpan header info.
Field Documentation
uint16_t InterPanHeader::clusterId |
uint16_t InterPanHeader::groupId |
bool InterPanHeader::hasLongAddress |
EmberEUI64 InterPanHeader::longAddress |
uint8_t InterPanHeader::messageType |
uint16_t InterPanHeader::panId |
uint16_t InterPanHeader::profileId |
EmberNodeId InterPanHeader::shortAddress |
The documentation for this struct was generated from the following files:
ami-inter-pan.h
ami-inter-pan-host.h