Bootloader GPIO definitions.
Enumerations | |
enum | blState_e { BL_ST_UP, BL_ST_DOWN, BL_ST_POLLING_LOOP, BL_ST_DOWNLOAD_LOOP, BL_ST_DOWNLOAD_FAILURE, BL_ST_DOWNLOAD_SUCCESS } |
Defines various bootloader states. Use in LED code to signal bootload activity. |
Functions | |
void | bootloadGpioInit (void) |
Initialize GPIO. | |
void | bootloadStateIndicator (enum blState_e state) |
Helper function used for displaying bootloader state (for example: with LEDs). | |
bool | bootloadForceActivation (void) |
Force activation of bootloader. |
State Indicator Macros | |
The bootloader indicates which state it is in by calling these // macros. Map them to the ::halBootloadStateIndicator function // (in bootloder-gpio.c) if you want to display that bootloader state. // Used to blink the LED's or otherwise signal bootloader activity. | |
#define | BL_STATE_UP() do { bootloadStateIndicator(BL_ST_UP); } while (0) |
Finished init sequence, ready for bootload. | |
#define | BL_STATE_DOWN() do { bootloadStateIndicator(BL_ST_DOWN); } while (0) |
Called right before bootloader resets to application. Use to cleanup and reset GPIO's to leave node in known state for app start, if necessary. | |
#define | BL_STATE_POLLING_LOOP() do { bootloadStateIndicator(BL_ST_POLLING_LOOP); } while (0) |
Standalone bootloader polling serial/radio interface. | |
#define | BL_STATE_DOWNLOAD_LOOP() do { bootloadStateIndicator(BL_ST_DOWNLOAD_LOOP); } while (0) |
Processing download image. | |
#define | BL_STATE_DOWNLOAD_SUCCESS() do { bootloadStateIndicator(BL_ST_DOWNLOAD_SUCCESS); } while (0) |
Download process was a success. | |
#define | BL_STATE_DOWNLOAD_FAILURE() do { bootloadStateIndicator(BL_ST_DOWNLOAD_FAILURE); } while (0) |
Download process failed. |
Detailed Description
Bootloader GPIO definitions.
See bootloader-gpio.h
for source code.
Macro Definition Documentation
#define BL_STATE_DOWN | ( |
| ) | do { bootloadStateIndicator(BL_ST_DOWN); } while (0) |
Called right before bootloader resets to application. Use to cleanup and reset GPIO's to leave node in known state for app start, if necessary.
#define BL_STATE_DOWNLOAD_FAILURE | ( |
| ) | do { bootloadStateIndicator(BL_ST_DOWNLOAD_FAILURE); } while (0) |
Download process failed.
#define BL_STATE_DOWNLOAD_LOOP | ( |
| ) | do { bootloadStateIndicator(BL_ST_DOWNLOAD_LOOP); } while (0) |
Processing download image.
#define BL_STATE_DOWNLOAD_SUCCESS | ( |
| ) | do { bootloadStateIndicator(BL_ST_DOWNLOAD_SUCCESS); } while (0) |
Download process was a success.
#define BL_STATE_POLLING_LOOP | ( |
| ) | do { bootloadStateIndicator(BL_ST_POLLING_LOOP); } while (0) |
Standalone bootloader polling serial/radio interface.
#define BL_STATE_UP | ( |
| ) | do { bootloadStateIndicator(BL_ST_UP); } while (0) |
Finished init sequence, ready for bootload.
Enumeration Type Documentation
enum blState_e |
Function Documentation
bool bootloadForceActivation | ( | void |
| ) |
Force activation of bootloader.
void bootloadGpioInit | ( | void |
| ) |
Initialize GPIO.
void bootloadStateIndicator | ( | enum blState_e | state | ) |
Helper function used for displaying bootloader state (for example: with LEDs).