ZigBee Device Object
Functions | |
EmberStatus | emberNetworkAddressRequest (EmberEUI64 target, bool reportKids, uint8_t childStartIndex) |
Requests the 16 bit network address of a node whose EUI64 is known. | |
EmberStatus | emberIeeeAddressRequest (EmberNodeId target, bool reportKids, uint8_t childStartIndex, EmberApsOption options) |
Requests the EUI64 of a node whose 16 bit network address is known. | |
EmberStatus | emberIeeeAddressRequestToTarget (EmberNodeId discoveryNodeId, bool reportKids, uint8_t childStartIndex, EmberApsOption options, EmberNodeId targetNodeIdOfRequest) |
EmberStatus | emberEnergyScanRequest (EmberNodeId target, uint32_t scanChannels, uint8_t scanDuration, uint16_t scanCount) |
Requests that an energy scan be performed and its results returned. This request may only be sent by the current network manager and must be unicast, not broadcast. | |
EmberStatus | emberSetNetworkManagerRequest (EmberNodeId networkManager, uint32_t activeChannels) |
Broadcasts a request to set the identity of the network manager and the active channel mask. The mask is used when scanning for the network after missing a channel update. | |
EmberStatus | emberChannelChangeRequest (uint8_t channel) |
Broadcasts a request to change the channel. This request may only be sent by the current network manager. A several second delay occurs from receipt of the broadcast to changing the channel to allow time for the broadcast to propagate. | |
EmberStatus | emberSendDeviceAnnouncement (void) |
Sends a broadcast for a ZDO Device announcement. Normally, it is NOT required to call this as the stack automatically sends a device announcement during joining or rejoining, as per the spec. | |
EmberStatus | emberSendParentAnnouncement (void) |
Sends a broadcast for a ZDO Parent Announcement. Normally, it is NOT required to call this as the stack automatically sends a Parent Announce when a Zigbee Router/Coordinator reboots, is in a joined or authenticated state, and has at least one device. | |
uint8_t | emberGetLastStackZigDevRequestSequence (void) |
Provides access to the stack ZDO transaction sequence number for the last request. |
Detailed Description
See zigbee-device-stack.h
for source code.
Function Documentation
EmberStatus emberChannelChangeRequest | ( | uint8_t | channel | ) |
Broadcasts a request to change the channel. This request may only be sent by the current network manager. A several second delay occurs from receipt of the broadcast to changing the channel to allow time for the broadcast to propagate.
- Parameters
-
channel
The channel to change to.
- Returns
- An
EmberStatus
value.
EmberStatus emberEnergyScanRequest | ( | EmberNodeId | target, |
uint32_t | scanChannels, |
||
uint8_t | scanDuration, |
||
uint16_t | scanCount |
||
) |
Requests that an energy scan be performed and its results returned. This request may only be sent by the current network manager and must be unicast, not broadcast.
- Parameters
-
target
The network address of the node to perform the scan. scanChannels
A mask of the channels to be scanned. scanDuration
How long to scan on each channel. Allowed values are 0..5, with the scan times as specified by 802.15.4 (0 = 31 ms, 1 = 46 ms, 2 = 77 ms, 3 = 138 ms, 4 = 261 ms, 5 = 507 ms). scanCount
The number of scans to be performed on each channel (1 .. 8).
- Returns
- An
EmberStatus
value.
uint8_t emberGetLastStackZigDevRequestSequence | ( | void |
| ) |
Provides access to the stack ZDO transaction sequence number for the last request.
- Returns
- The last stack ZDO transaction sequence number used.
EmberStatus emberIeeeAddressRequest | ( | EmberNodeId | target, |
bool | reportKids, |
||
uint8_t | childStartIndex, |
||
EmberApsOption | options |
||
) |
Requests the EUI64 of a node whose 16 bit network address is known.
- Parameters
-
target
The network address of the node. reportKids
True to request that the target list their children in the response. childStartIndex
The index of the first child to list in the response. Ignored if reportKids is false. options
The options to use when sending the request. See emberSendUnicast() for a description.
- Returns
- An
EmberStatus
value.
EmberStatus emberIeeeAddressRequestToTarget | ( | EmberNodeId | discoveryNodeId, |
bool | reportKids, |
||
uint8_t | childStartIndex, |
||
EmberApsOption | options, |
||
EmberNodeId | targetNodeIdOfRequest |
||
) |
EmberStatus emberNetworkAddressRequest | ( | EmberEUI64 | target, |
bool | reportKids, |
||
uint8_t | childStartIndex |
||
) |
Requests the 16 bit network address of a node whose EUI64 is known.
- Parameters
-
target
The EUI64 of the node. reportKids
True to request that the target list their children in the response. childStartIndex
The index of the first child to list in the response. Ignored if reportKids
is false.
- Returns
- An
EmberStatus
value.- EMBER_SUCCESS - The request was transmitted successfully.
- EMBER_NO_BUFFERS - Insufficient message buffers were available to construct the request.
- EMBER_NETWORK_DOWN - The node is not part of a network.
- EMBER_NETWORK_BUSY - Transmission of the request failed.
EmberStatus emberSendDeviceAnnouncement | ( | void |
| ) |
Sends a broadcast for a ZDO Device announcement. Normally, it is NOT required to call this as the stack automatically sends a device announcement during joining or rejoining, as per the spec.
May be used to re-send the device announcement.
- Returns
- An
EmberStatus
value.
EmberStatus emberSendParentAnnouncement | ( | void |
| ) |
Sends a broadcast for a ZDO Parent Announcement. Normally, it is NOT required to call this as the stack automatically sends a Parent Announce when a Zigbee Router/Coordinator reboots, is in a joined or authenticated state, and has at least one device.
May be used to re-send the parent announcement.
- Returns
- An
EmberStatus
value.
EmberStatus emberSetNetworkManagerRequest | ( | EmberNodeId | networkManager, |
uint32_t | activeChannels |
||
) |
Broadcasts a request to set the identity of the network manager and the active channel mask. The mask is used when scanning for the network after missing a channel update.
- Parameters
-
networkManager
The network address of the network manager. activeChannels
The new active channel mask.
- Returns
- An
EmberStatus
value.