EmberVersion Struct Reference
A version structure containing all version information.
#include <
ember-types.h
>
Data Fields | |
uint16_t | build |
uint8_t | major |
uint8_t | minor |
uint8_t | patch |
uint8_t | special |
EmberVersionType | type |
A version structure containing all version information.
Field Documentation
uint16_t EmberVersion::build |
uint8_t EmberVersion::major |
uint8_t EmberVersion::minor |
uint8_t EmberVersion::patch |
uint8_t EmberVersion::special |
EmberVersionType EmberVersion::type |
The documentation for this struct was generated from the following file:
ember-types.h