EmberMultiprotocolPriorities Struct Reference
#include <
ember-types.h
>
Data Fields | |
uint8_t | backgroundRx |
uint8_t | tx |
uint8_t | activeRx |
@ brief Struct used to specify priorities for zigbee radio operations in multiprotocol
Field Documentation
uint8_t EmberMultiprotocolPriorities::activeRx |
The priority of a Zigbee RX operation while receiving a packet.
uint8_t EmberMultiprotocolPriorities::backgroundRx |
The priority of a Zigbee RX operation while not receiving a packet.
uint8_t EmberMultiprotocolPriorities::tx |
The priority of a Zigbee TX operation.
The documentation for this struct was generated from the following file:
ember-types.h