Common bootloader serial definitions.
Functions | |
void | serInit (void) |
Initialize serial port. | |
void | serPutFlush (void) |
Flush the transmiter. | |
void | serPutChar (uint8_t ch) |
Transmit a character. | |
void | serPutStr (const char *str) |
Transmit a string. | |
void | serPutBuf (const uint8_t buf[], uint8_t size) |
Transmit a buffer. | |
void | serPutDecimal (uint16_t val) |
Transmit a 16bit value in decimal. | |
void | serPutHex (uint8_t byte) |
Transmit a byte as hex. | |
void | serPutHexInt (uint16_t word) |
Transmit a 16bit integer as hex. | |
bool | serCharAvailable (void) |
Determine if a character is available. | |
uint8_t | serGetChar (uint8_t *ch) |
Get a character if available, otherwise return an error. | |
void | serGetFlush (void) |
Flush the receiver. |
Detailed Description
Common bootloader serial definitions.
See bootloader-serial.h
for source code.
Function Documentation
bool serCharAvailable | ( | void |
| ) |
Determine if a character is available.
- Returns
- true if a character is available, false otherwise.
uint8_t serGetChar | ( | uint8_t * | ch | ) |
Get a character if available, otherwise return an error.
- Parameters
-
ch
Pointer to a location where the received byte will be placed.
- Returns
- BL_SUCCESS if a character was obtained, BL_ERR otherwise.
void serGetFlush | ( | void |
| ) |
Flush the receiver.
void serInit | ( | void |
| ) |
Initialize serial port.
void serPutBuf | ( | const uint8_t | buf[], |
uint8_t | size |
||
) |
Transmit a buffer.
- Parameters
-
buf
A buffer. size
Length of buffer.
void serPutChar | ( | uint8_t | ch | ) |
Transmit a character.
- Parameters
-
ch
A character.
void serPutDecimal | ( | uint16_t | val | ) |
Transmit a 16bit value in decimal.
- Parameters
-
val
The data to print.
void serPutFlush | ( | void |
| ) |
Flush the transmiter.
void serPutHex | ( | uint8_t | byte | ) |
Transmit a byte as hex.
- Parameters
-
byte
A byte.
void serPutHexInt | ( | uint16_t | word | ) |
Transmit a 16bit integer as hex.
- Parameters
-
word
A 16bit integer.
void serPutStr | ( | const char * | str | ) |
Transmit a string.
- Parameters
-
str
A string.