Data structure of the key_refresh_phase_status event.
Public Attribute Documentation#
result#
uint16_t sl_btmesh_evt_config_client_key_refresh_phase_status_s::result
SL_STATUS_OK if successful. Error code otherwise.
Definition at line
8765
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
handle#
uint32_t sl_btmesh_evt_config_client_key_refresh_phase_status_s::handle
Request handle
Definition at line
8766
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
netkey_index#
uint16_t sl_btmesh_evt_config_client_key_refresh_phase_status_s::netkey_index
Network key index for which the state applies
Definition at line
8767
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
value#
uint8_t sl_btmesh_evt_config_client_key_refresh_phase_status_s::value
Key refresh phase state of the node for the given network key. Valid values are:
0: Normal operation
1: First phase of key refresh procedure
2: Second phase of key refresh procedure
Definition at line
8768
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h