Data structure of the upload_failed event.
Public Attribute Documentation#
elem_index#
uint16_t sl_btmesh_evt_fw_dist_server_upload_failed_s::elem_index
Server model element index
Definition at line
17586
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
client_address#
uint16_t sl_btmesh_evt_fw_dist_server_upload_failed_s::client_address
Address of the Distribution Client
Definition at line
17587
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
size#
uint32_t sl_btmesh_evt_fw_dist_server_upload_failed_s::size
Upload size
Definition at line
17588
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
blob_id#
sl_bt_uuid_64_t sl_btmesh_evt_fw_dist_server_upload_failed_s::blob_id
BLOB ID
Definition at line
17589
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
fwid#
uint8array sl_btmesh_evt_fw_dist_server_upload_failed_s::fwid
FWID of the firmware image
Definition at line
17590
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h