displaypal.h File Reference
Platform Abstraction Layer (PAL) interface for DISPLAY driver.
- Version
- 5.4.0
License
Copyright 2015 Silicon Labs, Inc. http://www.silabs.com
This file is licensed under the Silabs License Agreement. See the file "Silabs_License_Agreement.txt" for details. Before using this software for any purpose, you must agree to the terms of that agreement.
Definition in file
displaypal.h
.
#include "
emstatus.h
"
Macros |
|
| #define | PAL_EMSTATUS_INVALID_PARAM ( PAL_EMSTATUS_BASE | 1) |
| #define | PAL_EMSTATUS_OK (0) |
| #define | PAL_EMSTATUS_REPEAT_FAILED ( PAL_EMSTATUS_BASE | 2) |
Macro Definition Documentation
| #define PAL_EMSTATUS_INVALID_PARAM ( PAL_EMSTATUS_BASE | 1) |
Invalid parameter.
Definition at line
31
of file
displaypal.h
.
| #define PAL_EMSTATUS_OK (0) |
EMSTATUS codes of the PAL interface. Operation successful.
Definition at line
30
of file
displaypal.h
.
| #define PAL_EMSTATUS_REPEAT_FAILED ( PAL_EMSTATUS_BASE | 2) |
Repeat failed.
Definition at line
32
of file
displaypal.h
.