retargettft.c File Reference
Provide stdio retargeting to TFT address mapped mode.
- Version
- 5.4.0
License
Copyright 2015 Silicon Labs, Inc. http://www.silabs.com
This file is licensed under the Silabs License Agreement. See the file "Silabs_License_Agreement.txt" for details. Before using this software for any purpose, you must agree to the terms of that agreement.
Definition in file
retargettft.c
.
#include <stdio.h>
#include <stdint.h>
#include "
em_device.h
"
#include "
em_cmu.h
"
#include "
em_ebi.h
"
#include "
em_gpio.h
"
#include "dmd/ssd2119/dmd_ssd2119.h"
#include "
bsp.h
"
#include "retargettft.h"
#include "
displayfont8x8.h
"
Macros |
|
| #define | CHARS 40 |
| #define | fontBits chars_8x8_bits |
| #define | LINES 30 |
Functions |
|
| int | RETARGET_ReadChar (void) |
|
Receive a byte No input method from TFT is possible, thus we always return -1.
|
|
| void | RETARGET_TftCrLf (int on) |
|
Toggle LF to CRLF conversion.
|
|
| void | RETARGET_TftInit (void) |
|
Intializes TFT text display.
|
|
| void | RETARGET_TFTTX (int c) |
|
Transmit/display a character.
|
|
| void | RETARGET_TFTUpdate (bool fullFrame) |
|
Display framebuffer.
|
|
| int | RETARGET_WriteChar (char c) |
|
Transmit single byte to the TFT.
|
|
| static void | tftTextReset (void) |
|
Reset TFT text display state.
|
|
| static void | tftTextScrollUp (void) |
|
Scroll one line of characters up on the screen.
|
|
Variables |
|
| static bool | bufferReset = true |
| static uint8_t | charBuffer [ LINES ][ CHARS ] |
| static bool | fullUpdate = true |
| static bool | initialized = false |
| static bool | LFtoCRLF = 0 |
| static uint8_t | rgbColor [3] |
| static bool | tftReset = true |
| static int | xpos |
| static int | ypos |
Macro Definition Documentation
| #define CHARS 40 |
Characters
Definition at line
29
of file
retargettft.c
.
Referenced by RETARGET_TFTTX() , RETARGET_TFTUpdate() , tftTextReset() , and tftTextScrollUp() .
| #define fontBits chars_8x8_bits |
| #define LINES 30 |
Lines
Definition at line
30
of file
retargettft.c
.
Referenced by RETARGET_TFTTX() , RETARGET_TFTUpdate() , tftTextReset() , and tftTextScrollUp() .
Variable Documentation
|
static |
Reset buffer
Definition at line
39
of file
retargettft.c
.
Referenced by RETARGET_WriteChar() , and tftTextReset() .
Character buffer
Definition at line
32
of file
retargettft.c
.
Referenced by RETARGET_TFTTX() , RETARGET_TFTUpdate() , tftTextReset() , and tftTextScrollUp() .
|
static |
Display updated
Definition at line
38
of file
retargettft.c
.
Referenced by RETARGET_WriteChar() , and tftTextScrollUp() .
|
static |
Intialize TFT stdio retarget
Definition at line
42
of file
retargettft.c
.
Referenced by RETARGET_WriteChar() , and tftTextReset() .
|
static |
LF to CRLF conversion disabled
Definition at line
41
of file
retargettft.c
.
Referenced by RETARGET_TftCrLf() , and RETARGET_WriteChar() .
|
static |
Color for font
Definition at line
33
of file
retargettft.c
.
Referenced by RETARGET_TFTTX() , RETARGET_TFTUpdate() , and tftTextReset() .
|
static |
Reset TFT
Definition at line
40
of file
retargettft.c
.
Referenced by RETARGET_WriteChar() , and tftTextReset() .
|
static |
Cursor position
Definition at line
36
of file
retargettft.c
.
Referenced by RETARGET_TFTTX() , RETARGET_TFTUpdate() , tftTextReset() , and tftTextScrollUp() .
|
static |
Cursor position
Definition at line
36
of file
retargettft.c
.
Referenced by RETARGET_TFTTX() , RETARGET_TFTUpdate() , tftTextReset() , and tftTextScrollUp() .