spidrv.c File Reference
SPIDRV API implementation.
- Version
- 5.4.0
License
(C) Copyright 2015 Silicon Labs, www.silabs.com
This file is licensed under the Silabs License Agreement. See the file "Silabs_License_Agreement.txt" for details. Before using this software for any purpose, you must agree to the terms of that agreement.
Definition in file spidrv.c
.
#include <string.h>
#include "em_device.h
"
#include "em_gpio.h
"
#include "em_core.h
"
#include "em_usart.h
"
#include "dmadrv.h
"
#include "spidrv.h
"
Functions | |
Ecode_t | SPIDRV_AbortTransfer (SPIDRV_Handle_t handle) |
Abort an ongoing SPI transfer. | |
Ecode_t | SPIDRV_DeInit (SPIDRV_Handle_t handle) |
Deinitialize an SPI driver instance. | |
Ecode_t | SPIDRV_GetBitrate (SPIDRV_Handle_t handle, uint32_t *bitRate) |
Get current SPI bus bitrate. | |
Ecode_t | SPIDRV_GetFramelength (SPIDRV_Handle_t handle, uint32_t *frameLength) |
Get current SPI framelength. | |
Ecode_t | SPIDRV_GetTransferStatus (SPIDRV_Handle_t handle, int *itemsTransferred, int *itemsRemaining) |
Get the status of an SPI transfer. | |
Ecode_t | SPIDRV_Init (SPIDRV_Handle_t handle, SPIDRV_Init_t *initData) |
Initialize an SPI driver instance. | |
Ecode_t | SPIDRV_MReceive (SPIDRV_Handle_t handle, void *buffer, int count, SPIDRV_Callback_t callback) |
Start an SPI master receive transfer. | |
Ecode_t | SPIDRV_MReceiveB (SPIDRV_Handle_t handle, void *buffer, int count) |
Start an SPI master blocking receive transfer. | |
Ecode_t | SPIDRV_MTransfer (SPIDRV_Handle_t handle, const void *txBuffer, void *rxBuffer, int count, SPIDRV_Callback_t callback) |
Start an SPI master transfer. | |
Ecode_t | SPIDRV_MTransferB (SPIDRV_Handle_t handle, const void *txBuffer, void *rxBuffer, int count) |
Start an SPI master blocking transfer. | |
Ecode_t | SPIDRV_MTransferSingleItemB (SPIDRV_Handle_t handle, uint32_t txValue, void *rxValue) |
Start an SPI master blocking single item (frame) transfer. | |
Ecode_t | SPIDRV_MTransmit (SPIDRV_Handle_t handle, const void *buffer, int count, SPIDRV_Callback_t callback) |
Start an SPI master transmit transfer. | |
Ecode_t | SPIDRV_MTransmitB (SPIDRV_Handle_t handle, const void *buffer, int count) |
Start an SPI master blocking transmit transfer. | |
Ecode_t | SPIDRV_SetBitrate (SPIDRV_Handle_t handle, uint32_t bitRate) |
Set SPI bus bitrate. | |
Ecode_t | SPIDRV_SetFramelength (SPIDRV_Handle_t handle, uint32_t frameLength) |
Set SPI framelength. | |
Ecode_t | SPIDRV_SReceive (SPIDRV_Handle_t handle, void *buffer, int count, SPIDRV_Callback_t callback, int timeoutMs) |
Start an SPI slave receive transfer. | |
Ecode_t | SPIDRV_SReceiveB (SPIDRV_Handle_t handle, void *buffer, int count, int timeoutMs) |
Start an SPI slave blocking receive transfer. | |
Ecode_t | SPIDRV_STransfer (SPIDRV_Handle_t handle, const void *txBuffer, void *rxBuffer, int count, SPIDRV_Callback_t callback, int timeoutMs) |
Start an SPI slave transfer. | |
Ecode_t | SPIDRV_STransferB (SPIDRV_Handle_t handle, const void *txBuffer, void *rxBuffer, int count, int timeoutMs) |
Start an SPI slave blocking transfer. | |
Ecode_t | SPIDRV_STransmit (SPIDRV_Handle_t handle, const void *buffer, int count, SPIDRV_Callback_t callback, int timeoutMs) |
Start an SPI slave transmit transfer. | |
Ecode_t | SPIDRV_STransmitB (SPIDRV_Handle_t handle, const void *buffer, int count, int timeoutMs) |
Start an SPI slave blocking transmit transfer. | |