CALIBRATE_TypeDef Struct ReferenceDevices > EZR32WG_CALIBRATE

Definition at line 49 of file ezr32wg_calibrate.h .

Data Fields

__IM uint32_t ADDRESS
__IM uint32_t VALUE

Field Documentation

__IM uint32_t CALIBRATE_TypeDef::ADDRESS

Address of calibration register

Definition at line 50 of file ezr32wg_calibrate.h .

__IM uint32_t CALIBRATE_TypeDef::VALUE

Default value for calibration register

Definition at line 51 of file ezr32wg_calibrate.h .


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EZR32WG/Include/ ezr32wg_calibrate.h