OPAMP_Init_TypeDef Struct ReferenceEMLIB > OPAMP
OPAMP init structure.
Definition at line
437
of file
em_opamp.h
.
#include <
em_opamp.h
>
Data Fields |
|
| uint32_t | bias |
| bool | defaultOffset |
| bool | halfBias |
| bool | hcmDisable |
| bool | lpfNegPadDisable |
| bool | lpfPosPadDisable |
| OPAMP_NegSel_TypeDef | negSel |
| bool | nextOut |
| bool | npEn |
| uint32_t | offset |
| OPAMP_OutMode_TypeDef | outMode |
| uint32_t | outPen |
| OPAMP_PosSel_TypeDef | posSel |
| bool | ppEn |
| OPAMP_ResInMux_TypeDef | resInMux |
| OPAMP_ResSel_TypeDef | resSel |
| bool | shortInputs |
Field Documentation
| uint32_t OPAMP_Init_TypeDef::bias |
| bool OPAMP_Init_TypeDef::defaultOffset |
Use factory calibrated opamp offset value.
Definition at line
497
of file
em_opamp.h
.
Referenced by OPAMP_Enable() .
| bool OPAMP_Init_TypeDef::halfBias |
Divide OPAMP bias current by 2.
Definition at line
489
of file
em_opamp.h
.
Referenced by OPAMP_Enable() .
| bool OPAMP_Init_TypeDef::hcmDisable |
Disable input rail-to-rail capability.
Definition at line
496
of file
em_opamp.h
.
Referenced by OPAMP_Enable() .
| bool OPAMP_Init_TypeDef::lpfNegPadDisable |
Disable low pass filter on negative pad.
Definition at line
491
of file
em_opamp.h
.
Referenced by OPAMP_Enable() .
| bool OPAMP_Init_TypeDef::lpfPosPadDisable |
Disable low pass filter on positive pad.
Definition at line
490
of file
em_opamp.h
.
Referenced by OPAMP_Enable() .
| OPAMP_NegSel_TypeDef OPAMP_Init_TypeDef::negSel |
Select input source for negative terminal.
Definition at line
438
of file
em_opamp.h
.
Referenced by OPAMP_Enable() .
| bool OPAMP_Init_TypeDef::nextOut |
Enable NEXTOUT signal source.
Definition at line
492
of file
em_opamp.h
.
Referenced by OPAMP_Enable() .
| bool OPAMP_Init_TypeDef::npEn |
| uint32_t OPAMP_Init_TypeDef::offset |
Opamp offset value when defaultOffset is false.
Definition at line
498
of file
em_opamp.h
.
Referenced by OPAMP_Enable() .
| OPAMP_OutMode_TypeDef OPAMP_Init_TypeDef::outMode |
Output terminal connection.
Definition at line
440
of file
em_opamp.h
.
Referenced by OPAMP_Enable() .
| uint32_t OPAMP_Init_TypeDef::outPen |
Alternate output enable bit mask. This value should consist of one or more of the DAC_OPA[opa#]MUX_OUTPEN_OUT[output#] flags (defined in <part_name>_dac.h) OR'ed together.
For OPA0:
- DAC_OPA0MUX_OUTPEN_OUT0
- DAC_OPA0MUX_OUTPEN_OUT1
- DAC_OPA0MUX_OUTPEN_OUT2
- DAC_OPA0MUX_OUTPEN_OUT3
- DAC_OPA0MUX_OUTPEN_OUT4
For OPA1:
- DAC_OPA1MUX_OUTPEN_OUT0
- DAC_OPA1MUX_OUTPEN_OUT1
- DAC_OPA1MUX_OUTPEN_OUT2
- DAC_OPA1MUX_OUTPEN_OUT3
- DAC_OPA1MUX_OUTPEN_OUT4
For OPA2:
- DAC_OPA2MUX_OUTPEN_OUT0
- DAC_OPA2MUX_OUTPEN_OUT1
E.g:
init.outPen = DAC_OPA0MUX_OUTPEN_OUT0 | DAC_OPA0MUX_OUTPEN_OUT2 | DAC_OPA0MUX_OUTPEN_OUT4;
Definition at line
443
of file
em_opamp.h
.
Referenced by OPAMP_Enable() .
| OPAMP_PosSel_TypeDef OPAMP_Init_TypeDef::posSel |
Select input source for positive terminal.
Definition at line
439
of file
em_opamp.h
.
Referenced by OPAMP_Enable() .
| bool OPAMP_Init_TypeDef::ppEn |
| OPAMP_ResInMux_TypeDef OPAMP_Init_TypeDef::resInMux |
Select input source for resistor ladder.
Definition at line
442
of file
em_opamp.h
.
Referenced by OPAMP_Enable() .
| OPAMP_ResSel_TypeDef OPAMP_Init_TypeDef::resSel |
Select R2/R1 resistor ratio.
Definition at line
441
of file
em_opamp.h
.
Referenced by OPAMP_Enable() .
| bool OPAMP_Init_TypeDef::shortInputs |
Short OPAMP input terminals.
Definition at line
495
of file
em_opamp.h
.
Referenced by OPAMP_Enable() .
The documentation for this struct was generated from the following file:
-
C:/repos/embsw_super_h1/platform/emlib/inc/
em_opamp.h