USBH_Device_TypeDef Struct ReferencePlatform Middleware > USB > USB_HOST
USB HOST device definition.
A host application should not manipulate the contents of this struct.
Definition at line
859
of file
em_usb.h
.
#include <
em_usb.h
>
Data Fields |
|
| uint8_t | addr |
| USB_ConfigurationDescriptor_TypeDef | confDesc |
| USB_DeviceDescriptor_TypeDef | devDesc |
| USBH_Ep_TypeDef * | ep |
| USBH_Ep_TypeDef | ep0 |
| USB_InterfaceDescriptor_TypeDef | itfDesc |
| int | numEp |
| uint8_t | speed |
Field Documentation
| uint8_t USBH_Device_TypeDef::addr |
The device address.
Definition at line
866
of file
em_usb.h
.
Referenced by USBH_InitDeviceData() , and USBH_SetAddressB() .
| USB_ConfigurationDescriptor_TypeDef USBH_Device_TypeDef::confDesc |
The device configuration descriptor.
Definition at line
861
of file
em_usb.h
.
Referenced by USBH_InitDeviceData() , and USBH_QueryDeviceB() .
| USB_DeviceDescriptor_TypeDef USBH_Device_TypeDef::devDesc |
The device device descriptor.
Definition at line
860
of file
em_usb.h
.
Referenced by USBH_InitDeviceData() , USBH_QueryDeviceB() , and USBH_WaitForDeviceConnectionB() .
| USBH_Ep_TypeDef * USBH_Device_TypeDef::ep |
Array of endpoint status data.
Definition at line
864
of file
em_usb.h
.
Referenced by USBH_InitDeviceData() , USBH_QueryDeviceB() , USBH_SetAltInterfaceB() , and USBH_SetConfigurationB() .
| USBH_Ep_TypeDef USBH_Device_TypeDef::ep0 |
Endpoint 0 status data.
Definition at line
863
of file
em_usb.h
.
Referenced by USBH_GetConfigurationDescriptorB() , USBH_GetDeviceDescriptorB() , USBH_GetStringB() , USBH_InitDeviceData() , USBH_QueryDeviceB() , USBH_SetAddressB() , USBH_SetAltInterfaceB() , USBH_SetConfigurationB() , USBH_StallEpB() , and USBH_UnStallEpB() .
| USB_InterfaceDescriptor_TypeDef USBH_Device_TypeDef::itfDesc |
The device interface descriptor.
Definition at line
862
of file
em_usb.h
.
Referenced by USBH_InitDeviceData() .
| int USBH_Device_TypeDef::numEp |
Number of endpoints.
Definition at line
865
of file
em_usb.h
.
Referenced by USBH_InitDeviceData() , USBH_SetAltInterfaceB() , and USBH_SetConfigurationB() .
| uint8_t USBH_Device_TypeDef::speed |
The device speed (low or full speed).
Definition at line
867
of file
em_usb.h
.
Referenced by MSDBOT_Init() , USBH_InitDeviceData() , and USBH_QueryDeviceB() .
The documentation for this struct was generated from the following file:
-
C:/repos/embsw_super_h1/platform/middleware/usb_gecko/inc/
em_usb.h