BURTC_RET_TypeDef Struct ReferenceDevices

BURTC_RET EZR32WG BURTC RET.

Definition at line 46 of file ezr32wg_burtc_ret.h .

#include < ezr32wg_burtc_ret.h >

Data Fields

__IOM uint32_t REG

Field Documentation

__IOM uint32_t BURTC_RET_TypeDef::REG

Retention Register

Definition at line 47 of file ezr32wg_burtc_ret.h .


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EZR32WG/Include/ ezr32wg_burtc_ret.h