ADC_InitScan_TypeDef Struct ReferenceEMLIB > ADC
Scan sequence init structure.
Definition at line
862
of file
em_adc.h
.
#include <
em_adc.h
>
Data Fields |
|
| ADC_AcqTime_TypeDef | acqTime |
| bool | diff |
| uint32_t | input |
| bool | leftAdjust |
| bool | prsEnable |
| ADC_PRSSEL_TypeDef | prsSel |
| ADC_Ref_TypeDef | reference |
| bool | rep |
| ADC_Res_TypeDef | resolution |
Field Documentation
| ADC_AcqTime_TypeDef ADC_InitScan_TypeDef::acqTime |
Acquisition time (in ADC clock cycles).
Definition at line
870
of file
em_adc.h
.
Referenced by ADC_InitScan() .
| bool ADC_InitScan_TypeDef::diff |
Select if single ended or differential input.
Definition at line
900
of file
em_adc.h
.
Referenced by ADC_InitScan() .
| uint32_t ADC_InitScan_TypeDef::input |
Scan input selection. If single ended (
diff
is false), use logical combination of ADC_SCANCTRL_INPUTMASK_CHx defines. If differential input (
diff
is true), use logical combination of ADC_SCANCTRL_INPUTMASK_CHxCHy defines. (Notice underscore prefix for defines used.)
Definition at line
888
of file
em_adc.h
.
Referenced by ADC_InitScan() .
| bool ADC_InitScan_TypeDef::leftAdjust |
Select if left adjustment should be done.
Definition at line
906
of file
em_adc.h
.
Referenced by ADC_InitScan() .
| bool ADC_InitScan_TypeDef::prsEnable |
Peripheral reflex system trigger enable.
Definition at line
903
of file
em_adc.h
.
Referenced by ADC_InitScan() , and MIC_init() .
| ADC_PRSSEL_TypeDef ADC_InitScan_TypeDef::prsSel |
Peripheral reflex system trigger selection. Only applicable if
prsEnable
is enabled.
Definition at line
867
of file
em_adc.h
.
Referenced by ADC_InitScan() , and MIC_init() .
| ADC_Ref_TypeDef ADC_InitScan_TypeDef::reference |
Sample reference selection. Notice that for external references, the ADC calibration register must be set explicitly.
Definition at line
876
of file
em_adc.h
.
Referenced by ADC_InitScan() , and MIC_init() .
| bool ADC_InitScan_TypeDef::rep |
Select if continuous conversion until explicit stop.
Definition at line
909
of file
em_adc.h
.
Referenced by ADC_InitScan() .
| ADC_Res_TypeDef ADC_InitScan_TypeDef::resolution |
The documentation for this struct was generated from the following file:
-
C:/repos/embsw_super_h1/platform/emlib/inc/
em_adc.h