LESENSE_DecCtrlDesc_TypeDef Struct ReferenceEMLIB > LESENSE

LESENSE decoder control descriptor structure.

Definition at line 671 of file em_lesense.h .

#include < em_lesense.h >

Data Fields

bool chkState
LESENSE_DecInput_TypeDef decInput
bool hystIRQ
bool hystPRS0
bool hystPRS1
bool hystPRS2
uint32_t initState
bool intMap
LESENSE_PRSSel_TypeDef prsChSel0
LESENSE_PRSSel_TypeDef prsChSel1
LESENSE_PRSSel_TypeDef prsChSel2
LESENSE_PRSSel_TypeDef prsChSel3
bool prsCount

Field Documentation

bool LESENSE_DecCtrlDesc_TypeDef::chkState

Set to enable the decoder to check the present state in addition to the states defined in TCONF.

Definition at line 680 of file em_lesense.h .

Referenced by LESENSE_Init() .

LESENSE_DecInput_TypeDef LESENSE_DecCtrlDesc_TypeDef::decInput

Select the input to the LESENSE decoder.

Definition at line 673 of file em_lesense.h .

Referenced by LESENSE_Init() .

bool LESENSE_DecCtrlDesc_TypeDef::hystIRQ

Set to enable hysteresis in the decoder for suppressing interrupt requests.

Definition at line 700 of file em_lesense.h .

Referenced by LESENSE_Init() .

bool LESENSE_DecCtrlDesc_TypeDef::hystPRS0

Set to enable hysteresis in the decoder for suppressing changes on PRS channel 0.

Definition at line 688 of file em_lesense.h .

Referenced by LESENSE_Init() .

bool LESENSE_DecCtrlDesc_TypeDef::hystPRS1

Set to enable hysteresis in the decoder for suppressing changes on PRS channel 1.

Definition at line 692 of file em_lesense.h .

Referenced by LESENSE_Init() .

bool LESENSE_DecCtrlDesc_TypeDef::hystPRS2

Set to enable hysteresis in the decoder for suppressing changes on PRS channel 2.

Definition at line 696 of file em_lesense.h .

Referenced by LESENSE_Init() .

uint32_t LESENSE_DecCtrlDesc_TypeDef::initState

Initial state of the LESENSE decoder.

Definition at line 676 of file em_lesense.h .

Referenced by LESENSE_Init() .

bool LESENSE_DecCtrlDesc_TypeDef::intMap

When set, a transition from state x in the decoder will set interrupt flag CHx.

Definition at line 684 of file em_lesense.h .

Referenced by LESENSE_Init() .

LESENSE_PRSSel_TypeDef LESENSE_DecCtrlDesc_TypeDef::prsChSel0

Select PRS channel input for bit 0 of the LESENSE decoder.

Definition at line 707 of file em_lesense.h .

Referenced by LESENSE_Init() .

LESENSE_PRSSel_TypeDef LESENSE_DecCtrlDesc_TypeDef::prsChSel1

Select PRS channel input for bit 1 of the LESENSE decoder.

Definition at line 710 of file em_lesense.h .

Referenced by LESENSE_Init() .

LESENSE_PRSSel_TypeDef LESENSE_DecCtrlDesc_TypeDef::prsChSel2

Select PRS channel input for bit 2 of the LESENSE decoder.

Definition at line 713 of file em_lesense.h .

Referenced by LESENSE_Init() .

LESENSE_PRSSel_TypeDef LESENSE_DecCtrlDesc_TypeDef::prsChSel3

Select PRS channel input for bit 3 of the LESENSE decoder.

Definition at line 716 of file em_lesense.h .

Referenced by LESENSE_Init() .

bool LESENSE_DecCtrlDesc_TypeDef::prsCount

Set to enable count mode on decoder PRS channels 0 and 1 to produce outputs which can be used by a PCNT to count up or down.

Definition at line 704 of file em_lesense.h .

Referenced by LESENSE_Init() .


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/emlib/inc/ em_lesense.h