USB_DIEP_TypeDef Struct ReferenceDevices

USB_DIEP EZR32WG USB DIEP.

Definition at line 46 of file ezr32wg_usb_diep.h .

#include < ezr32wg_usb_diep.h >

Data Fields

__IOM uint32_t CTL
__IOM uint32_t DMAADDR
__IOM uint32_t INT
uint32_t RESERVED0 [1]
uint32_t RESERVED1 [1]
uint32_t RESERVED2 [1]
__IOM uint32_t TSIZ
__IM uint32_t TXFSTS

Field Documentation

__IOM uint32_t USB_DIEP_TypeDef::CTL

Device IN Endpoint x+1 Control Register

Definition at line 47 of file ezr32wg_usb_diep.h .

__IOM uint32_t USB_DIEP_TypeDef::DMAADDR

Device IN Endpoint x+1 DMA Address Register

Definition at line 52 of file ezr32wg_usb_diep.h .

__IOM uint32_t USB_DIEP_TypeDef::INT

Device IN Endpoint x+1 Interrupt Register

Definition at line 49 of file ezr32wg_usb_diep.h .

uint32_t USB_DIEP_TypeDef::RESERVED0[1]

Reserved for future use

Definition at line 48 of file ezr32wg_usb_diep.h .

uint32_t USB_DIEP_TypeDef::RESERVED1[1]

Reserved for future use

Definition at line 50 of file ezr32wg_usb_diep.h .

uint32_t USB_DIEP_TypeDef::RESERVED2[1]

Reserved future

Definition at line 54 of file ezr32wg_usb_diep.h .

__IOM uint32_t USB_DIEP_TypeDef::TSIZ

Device IN Endpoint x+1 Transfer Size Register

Definition at line 51 of file ezr32wg_usb_diep.h .

__IM uint32_t USB_DIEP_TypeDef::TXFSTS

Device IN Endpoint x+1 Transmit FIFO Status Register

Definition at line 53 of file ezr32wg_usb_diep.h .


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EZR32WG/Include/ ezr32wg_usb_diep.h