EMU_VmonInit_TypeDef Struct ReferenceEMLIB > EMU
VMON initialization structure.
Definition at line
666
of file
em_emu.h
.
#include <
em_emu.h
>
Data Fields |
|
| EMU_VmonChannel_TypeDef | channel |
| bool | enable |
| bool | fallWakeup |
| bool | retDisable |
| bool | riseWakeup |
| int | threshold |
Field Documentation
| EMU_VmonChannel_TypeDef EMU_VmonInit_TypeDef::channel |
| bool EMU_VmonInit_TypeDef::enable |
| bool EMU_VmonInit_TypeDef::fallWakeup |
Wake up from EM4H on falling edge.
Definition at line
670
of file
em_emu.h
.
Referenced by EMU_VmonInit() .
| bool EMU_VmonInit_TypeDef::retDisable |
Disable IO0 retention when voltage drops below threshold (IOVDD only).
Definition at line
672
of file
em_emu.h
.
Referenced by EMU_VmonInit() .
| bool EMU_VmonInit_TypeDef::riseWakeup |
Wake up from EM4H on rising edge.
Definition at line
669
of file
em_emu.h
.
Referenced by EMU_VmonInit() .
| int EMU_VmonInit_TypeDef::threshold |
Trigger threshold (mV). Supported range is 1620 mV to 3400 mV.
Definition at line
668
of file
em_emu.h
.
Referenced by EMU_VmonInit() .
The documentation for this struct was generated from the following file:
-
C:/repos/embsw_super_h1/platform/emlib/inc/
em_emu.h