USART_InitIrDA_TypeDef Struct ReferenceEMLIB > USART
IrDA mode initialization structure. Inherited from asynchronous mode initialization structure.
Definition at line
560
of file
em_usart.h
.
#include <
em_usart.h
>
Data Fields |
|
| USART_InitAsync_TypeDef | async |
| bool | irFilt |
| bool | irPrsEn |
| USART_IrDAPrsSel_Typedef | irPrsSel |
| USART_IrDAPw_Typedef | irPw |
| bool | irRxInv |
Field Documentation
| USART_InitAsync_TypeDef USART_InitIrDA_TypeDef::async |
General Asynchronous initialization structure.
Definition at line
562
of file
em_usart.h
.
Referenced by USARTn_InitIrDA() .
| bool USART_InitIrDA_TypeDef::irFilt |
Set to enable filter on IrDA demodulator.
Definition at line
568
of file
em_usart.h
.
Referenced by USARTn_InitIrDA() .
| bool USART_InitIrDA_TypeDef::irPrsEn |
Enable the PRS channel selected by irPrsSel as input to IrDA module instead of TX.
Definition at line
576
of file
em_usart.h
.
Referenced by USARTn_InitIrDA() .
| USART_IrDAPrsSel_Typedef USART_InitIrDA_TypeDef::irPrsSel |
PRS can be used as input to the pulse modulator instead of TX. This value selects the channel to use.
Definition at line
580
of file
em_usart.h
.
Referenced by USARTn_InitIrDA() .
| USART_IrDAPw_Typedef USART_InitIrDA_TypeDef::irPw |
Configure the pulse width generated by the IrDA modulator as a fraction of the configured USART bit period.
Definition at line
572
of file
em_usart.h
.
Referenced by USARTn_InitIrDA() .
| bool USART_InitIrDA_TypeDef::irRxInv |
Set to invert Rx signal before IrDA demodulator.
Definition at line
565
of file
em_usart.h
.
Referenced by USARTn_InitIrDA() .
The documentation for this struct was generated from the following file:
-
C:/repos/embsw_super_h1/platform/emlib/inc/
em_usart.h