LESENSE_CoreCtrlDesc_TypeDef Struct ReferenceEMLIB > LESENSE
Core control (LESENSE_CTRL) descriptor structure.
       Definition at line
       
        489
       
       of file
       
        em_lesense.h
       
       .
      
      
       #include <
       
     
        em_lesense.h
       
       >
      
Field Documentation
| LESENSE_BiasMode_TypeDef LESENSE_CoreCtrlDesc_TypeDef::biasMode | 
| bool LESENSE_CoreCtrlDesc_TypeDef::bufOverWr | 
Set to true in order to always make LESENSE write to the result buffer, even if it is full.
        Definition at line
        
         514
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by LESENSE_Init() .
| LESENSE_BufTrigLevel_TypeDef LESENSE_CoreCtrlDesc_TypeDef::bufTrigLevel | 
Select trigger conditions for the interrupt and DMA.
        Definition at line
        
         517
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by LESENSE_Init() .
| bool LESENSE_CoreCtrlDesc_TypeDef::debugRun | 
Set to true to keep LESENSE running in the debug mode.
        Definition at line
        
         526
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by LESENSE_Init() .
| bool LESENSE_CoreCtrlDesc_TypeDef::dualSample | 
Set to true to sample both ACMPs simultaneously.
        Definition at line
        
         506
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by LESENSE_Init() .
| bool LESENSE_CoreCtrlDesc_TypeDef::invACMP0 | 
Set to true to invert ACMP0 output.
        Definition at line
        
         500
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by LESENSE_Init() .
| bool LESENSE_CoreCtrlDesc_TypeDef::invACMP1 | 
Set to true to invert ACMP1 output.
        Definition at line
        
         503
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by LESENSE_Init() .
| LESENSE_PRSSel_TypeDef LESENSE_CoreCtrlDesc_TypeDef::prsSel | 
Select PRS source for scan start if scanMode is set to lesensePrsPulse.
        Definition at line
        
         494
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by LESENSE_Init() .
| LESENSE_ScanConfSel_TypeDef LESENSE_CoreCtrlDesc_TypeDef::scanConfSel | 
Select scan configuration register usage strategy.
        Definition at line
        
         497
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by LESENSE_Init() .
| LESENSE_ScanMode_TypeDef LESENSE_CoreCtrlDesc_TypeDef::scanStart | 
Select scan start mode to control how the scan start is being triggered.
        Definition at line
        
         491
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by CAPLESENSE_setupLESENSE() , and LESENSE_Init() .
| bool LESENSE_CoreCtrlDesc_TypeDef::storeScanRes | 
Set to true in order to store SCANRES in the RAM (accessible via RESDATA) after each scan.
        Definition at line
        
         510
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by LESENSE_Init() .
| LESENSE_DMAWakeUp_TypeDef LESENSE_CoreCtrlDesc_TypeDef::wakeupOnDMA | 
Configure trigger condition for the DMA wakeup from EM2.
        Definition at line
        
         520
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by LESENSE_Init() .
The documentation for this struct was generated from the following file:
- 
       C:/repos/embsw_super_h1/platform/emlib/inc/
       em_lesense.h