LESENSE_AltExDesc_TypeDef Struct ReferenceEMLIB > LESENSE
Alternate excitation descriptor structure.
       Definition at line
       
        924
       
       of file
       
        em_lesense.h
       
       .
      
      
       #include <
       
     
        em_lesense.h
       
       >
      
| Data Fields | |
| bool | alwaysEx | 
| bool | enablePin | 
| LESENSE_AltExPinIdle_TypeDef | idleConf | 
Field Documentation
| bool LESENSE_AltExDesc_TypeDef::alwaysEx | 
Configure how to control external alternate excitation pins. Only applies if altExMap has been set to lesenseAltExMapALTEX. If true, excitation happens on the corresponding alternate excitation pin during excitation periods of all the enabled channels. If false, excitation happens on the corresponding alternate excitation pin ONLY during excitation period of the corresponding channel. The alwaysEx parameter is not valid when altExMap==lesenseAltExMapACMP.
        Definition at line
        
         940
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by LESENSE_AltExConfig() .
| bool LESENSE_AltExDesc_TypeDef::enablePin | 
Configure alternate excitation pins. If set, the corresponding alternate excitation pin/signal is enabled.
        Definition at line
        
         927
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by LESENSE_AltExConfig() .
| LESENSE_AltExPinIdle_TypeDef LESENSE_AltExDesc_TypeDef::idleConf | 
Configure idle phase setup of alternate excitation pins. The idleConf parameter is not valid when altExMap==lesenseAltExMapACMP.
        Definition at line
        
         931
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by LESENSE_AltExConfig() .
The documentation for this struct was generated from the following file:
- 
       C:/repos/embsw_super_h1/platform/emlib/inc/
       em_lesense.h