MSDBOT_CBW_TypeDef Struct ReferenceKit Drivers > Msd
Bulk Only Transport (BOT) Command Block Wrapper (CBW) typedef.
Definition at line
51
of file
msdbot.h
.
#include <
msdbot.h
>
Data Fields |
|
| union { | |
| struct { | |
| uint8_t CBLength : 5 | |
| uint8_t Reserved3 : 3 | |
| } | |
| uint8_t bCBWCBLength | |
| }; | |
| union { | |
| struct { | |
| uint8_t Direction : 1 | |
| uint8_t Obsolete : 1 | |
| uint8_t Reserved1 : 6 | |
| } | |
| uint8_t bmCBWFlags | |
| }; | |
| union { | |
| struct { | |
| uint8_t Lun : 4 | |
| uint8_t Reserved2 : 4 | |
| } | |
| uint8_t bCBWLUN | |
| }; | |
| uint8_t | CBWCB [16] |
| uint32_t | dCBWDataTransferLength |
| uint32_t | dCBWSignature |
| uint32_t | dCBWTag |
Field Documentation
| uint8_t MSDBOT_CBW_TypeDef::bCBWCBLength |
SCSI CDB length.
Definition at line
75
of file
msdbot.h
.
| uint8_t MSDBOT_CBW_TypeDef::bmCBWFlags |
CBW Flags.
Definition at line
61
of file
msdbot.h
.
| uint8_t MSDBOT_CBW_TypeDef::CBLength |
SCSI CDB length.
Definition at line
72
of file
msdbot.h
.
| uint8_t MSDBOT_CBW_TypeDef::CBWCB[16] |
| uint32_t MSDBOT_CBW_TypeDef::dCBWDataTransferLength |
| uint32_t MSDBOT_CBW_TypeDef::dCBWSignature |
The CBW signature (ascii USBC).
Definition at line
52
of file
msdbot.h
.
| uint32_t MSDBOT_CBW_TypeDef::dCBWTag |
The CBW tag.
Definition at line
53
of file
msdbot.h
.
| uint8_t MSDBOT_CBW_TypeDef::Direction |
BOT transfer directon, 1=BOT IN
Definition at line
59
of file
msdbot.h
.
Referenced by MSDBOT_Xfer() .
| uint8_t MSDBOT_CBW_TypeDef::Lun |
Device Logical Unit Number.
Definition at line
65
of file
msdbot.h
.
| uint8_t MSDBOT_CBW_TypeDef::Obsolete |
Obsolete, expect 0.
Definition at line
58
of file
msdbot.h
.
| uint8_t MSDBOT_CBW_TypeDef::Reserved1 |
Reserved, expect 0.
Definition at line
57
of file
msdbot.h
.
| uint8_t MSDBOT_CBW_TypeDef::Reserved2 |
Reserved, expect 0.
Definition at line
66
of file
msdbot.h
.
| uint8_t MSDBOT_CBW_TypeDef::Reserved3 |
Reserved, expect 0.
Definition at line
73
of file
msdbot.h
.
The documentation for this struct was generated from the following file:
-
C:/repos/embsw_super_h1/hardware/kit/common/drivers/
msdbot.h