Debug Utils RAM Dump#
1. Purpose / Scope#
This section provides examples to easily configure and execute debug applications of RS9116 module.
The RAM dump application is use to read the RAM content of RS9116W module for a given address.
2. Prerequisites / Setup Requirements#
Before running the application, the user will need the following things to setup.
2.1 Hardware Requirements#
- Windows PC with Host interface(UART/ SPI). 
- Silicon Labs RS9116 Wi-Fi Evaluation Kit 
- Host MCU Eval Kit. This example has been tested with: - Silicon Labs WSTK + EFR32MG21 
 


2.2 Software Requirements#
- Embedded Development Environment - For STM32, use licensed Keil IDE 
- For Silicon Labs EFx32, use the latest version of Simplicity Studio 
 
3. Application Build Environment#
3.1 Platform#
The Application can be built and executed on below Host platforms
3.2 Host Interface#
- By default, the application is configured to use the SPI bus for interfacing between Host platforms and the RS9116W EVK. 
- The SAPI driver provides APIs to enable other host interfaces if SPI is not suitable for your needs. 
3.3 Project Configuration#
The Application is provided with the project folder containing Keil and Simplicity Studio project files.
- Keil Project - The Keil project is used to evaluate the application on STM32. 
- Project path: - <SDK>/examples/snippets/debug_utils/ram_dump/projects/ram_dump-nucleo-f411re.uvprojx
 
- Simplicity Studio - The Simplicity Studio project is used to evaluate the application on EFR32MG21. 
- Project path: - If the Radio Board is BRD4180A or BRD4181A, then access the path - <SDK>/examples/snippets/debug_utils/ram_dump/projects/ram_dump-brd4180a-mg21.slsproj
- If the Radio Board is BRD4180B or BRD4181B, then access the path - <SDK>/examples/snippets/debug_utils/ram_dump/projects/ram_dump-brd4180b-mg21.slsproj- User can find the Radio Board version as given below 
 
 
 


3.4 Bare Metal Support#
This application supports only bare metal environment. By default, the application project files (Keil and Simplicity Studio) are provided with bare metal configuration.
4. Application Configuration Parameters#
The application can be configured to suit your requirements and development environment. Read through the following sections and make any changes needed.
4.1 Open rsi_ram_dump.c file and update/modify following macros,
Path : /examples/snippets/debug_utils/ram_dump
This define should be ENABLE only in case of linux platform with USB interface, by default, it is DISABLE
#define LINUX_PLATFORM         DISABLEAddress in Silicon Labs module
#define READ_ADDRESS           0x05. Testing the Application#
User has to follow the below steps for the successful execution of the application.
5.1 Loading the RS9116W Firmware#
Refer Getting started with PC  to load the firmware into RS9116W EVK. The firmware binary is located in <SDK>/firmware/
5.2 Building the Application on the Host Platform#
5.2.1 Using STM32#
Refer STM32 Getting Started
- Open the project - <SDK>/examples/snippets/debug_utils/ram_dump/projects/ram_dump-nucleo-f411re.uvprojxin Keil IDE.
- Build and Debug the project 
- Check for the RESET pin: - If RESET pin is connected from STM32 to RS9116W EVK, then user need not press the RESET button on RS9116W EVK before free run. 
- If RESET pin is not connected from STM32 to RS9116W EVK, then user need to press the RESET button on RS9116W EVK before free run. 
 
- Free run the project 
- Then continue the common steps from Section 5.3 
5.2.2 Using EFX32#
Refer EFx32 Getting Started
- Import the project from - <SDK>/examples/snippets/debug_utils/ram_dump/projects
- Select the appropriate .slsproj as per Radio Board type mentioned in Section 3.3 
- Compile and flash the project in to Host MCU 
- Debug the project 
- Check for the RESET pin: - If RESET pin is connected from STM32 to RS9116W EVK, then user need not press the RESET button on RS9116W EVK before free run 
- If RESET pin is not connected from STM32 to RS9116W EVK, then user need to press the RESET button on RS9116W EVK before free run 
 
- Free run the project 
- Then continue the common steps from Section 5.3 
5.3 Common Steps#
- Build and launch the application. 
- After the program gets executed RAM content is saved in ram_content buffer. In case of USB interface RAM content is saved in file dump.txt.