Structure represents the BLE operation mode.
This structure is used to define the parameters for the BLE operation mode, that includes Bluetooth features, and the module type.
Public Attribute Documentation#
bt_features#
uint32_t rsi_ble_oper_mode_s::bt_features
Bluetooth features.
Definition at line
428
of file components/device/silabs/si91x/wireless/ble/inc/rsi_bt_common.h
module_type#
uint8_t rsi_ble_oper_mode_s::module_type
Module type.
Definition at line
430
of file components/device/silabs/si91x/wireless/ble/inc/rsi_bt_common.h