Structure represents the Bluetooth set feature bitmap.

This structure is used to define the parameters for setting the Bluetooth feature bitmap, which includes feature bits in a bit map format.

Public Attributes#

uint32_t

Public Attribute Documentation#

bit_map#

uint32_t rsi_bt_set_feature_bitmap_s::bit_map

Features bits (bit map)


Definition at line 417 of file components/device/silabs/si91x/wireless/ble/inc/rsi_bt_common.h