Structure represents the Bluetooth set local Bluetooth Device (BD) address.

This structure is used to define the parameters for setting the local Bluetooth device address.

Public Attributes#

uint8_t

Device address (6 bytes)

Public Attribute Documentation#

dev_addr#

uint8_t rsi_bt_set_local_bd_addr_s::dev_addr[RSI_DEV_ADDR_LEN]

Device address (6 bytes)


Definition at line 500 of file components/device/silabs/si91x/wireless/ble/inc/rsi_bt_common.h