You are viewing documentation for version:
3.5.3 (latest)
PDF Structure represents the Bluetooth Packet Error Rate (PER) statistics.
This structure is used to define the parameters for collecting Bluetooth PER statistics, that includes counts of CRC fails, successful transmissions, and other relevant metrics.
Public Attribute Documentation# crc_fail_cnt# uint16_t rsi_bt_per_stats_s::crc_fail_cnt Packet count of CRC fails (Cyclic Redundancy Check (CRC))
crc_pass_cnt# uint16_t rsi_bt_per_stats_s::crc_pass_cnt Packet count of CRC passes
tx_abort_cnt# uint16_t rsi_bt_per_stats_s::tx_abort_cnt Packet count of aborted transmissions
rx_drop_cnt# uint16_t rsi_bt_per_stats_s::rx_drop_cnt Packet count of dropped receptions
rx_cca_idle_cnt# uint16_t rsi_bt_per_stats_s::rx_cca_idle_cnt Packet count of CCA Idle (Clear Channel Assessment (CCA))
rx_start_idle_cnt# uint16_t rsi_bt_per_stats_s::rx_start_idle_cnt Packet count of Rx start
rx_abrt_cnt# uint16_t rsi_bt_per_stats_s::rx_abrt_cnt Packet count of aborted receptions
tx_dones# uint16_t rsi_bt_per_stats_s::tx_dones Packet count of successful transmissions
rssi int8_t rsi_bt_per_stats_s::rssi Received Signal Strength Indicator of the packet
id_pkts_rcvd# uint16_t rsi_bt_per_stats_s::id_pkts_rcvd Packet count of ID packets received
dummy# uint16_t rsi_bt_per_stats_s::dummy[5] Dummy array of length 5