Structure represents the Bluetooth set antenna transmit power level.
This structure is used to define the parameters for setting the antenna transmit power level, which includes the protocol mode and transmit power.
Public Attribute Documentation#
protocol_mode#
uint8_t rsi_bt_set_antenna_tx_power_level_s::protocol_mode
Protocol mode: 1-BT, 2-LE.
Definition at line
456
of file components/device/silabs/si91x/wireless/ble/inc/rsi_bt_common.h
tx_power#
int8_t rsi_bt_set_antenna_tx_power_level_s::tx_power
Transmit power.
Definition at line
458
of file components/device/silabs/si91x/wireless/ble/inc/rsi_bt_common.h