You are viewing documentation for version:2.12.0PDFRequest message body. Public Attributes#uint8_tdataoption value int32_tlevelSocket protocol level. uint16_toption_lengthoption data length int32_toption_nameSocket option name. int32_tsocket_idID of the socket. Public Attribute Documentation#data#uint8_t sl_wisun_msg_set_socket_option_req_body_t::data[]option value level#int32_t sl_wisun_msg_set_socket_option_req_body_t::levelSocket protocol level. option_length#uint16_t sl_wisun_msg_set_socket_option_req_body_t::option_lengthoption data length option_name#int32_t sl_wisun_msg_set_socket_option_req_body_t::option_nameSocket option name. socket_id#int32_t sl_wisun_msg_set_socket_option_req_body_t::socket_idID of the socket.