You are viewing documentation for version:2.12.0PDFRequest message body. Public Attributes#uint8_tchannel_exclusion_modeChannel exclusion mode. uint16_tmtu_size6LoWPAN MTU size in bytes uint8_treservedReserved, set to zero. Public Attribute Documentation#channel_exclusion_mode#uint8_t sl_wisun_msg_set_tbu_settings_req_body_t::channel_exclusion_modeChannel exclusion mode. mtu_size#uint16_t sl_wisun_msg_set_tbu_settings_req_body_t::mtu_size6LoWPAN MTU size in bytes reserved#uint8_t sl_wisun_msg_set_tbu_settings_req_body_t::reservedReserved, set to zero.