Data structure of the appkey_status event.
Public Attribute Documentation#
result#
uint16_t sl_btmesh_evt_config_client_appkey_status_s::result
SL_STATUS_OK if successful. Error code otherwise.
Definition at line
8227
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
handle#
uint32_t sl_btmesh_evt_config_client_appkey_status_s::handle
Request handle
Definition at line
8228
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h