Data structure of the heartbeat_pub_status event.
Public Attribute Documentation#
result#
uint16_t sl_btmesh_evt_config_client_heartbeat_pub_status_s::result
SL_STATUS_OK if successful. Error code otherwise.
Definition at line
8495
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
handle#
uint32_t sl_btmesh_evt_config_client_heartbeat_pub_status_s::handle
Request handle
Definition at line
8497
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
destination_address#
uint16_t sl_btmesh_evt_config_client_heartbeat_pub_status_s::destination_address
Heartbeat publication destination address.
Definition at line
8498
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
netkey_index#
uint16_t sl_btmesh_evt_config_client_heartbeat_pub_status_s::netkey_index
Index of the network key used to encrypt heartbeat messages
Definition at line
8499
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
count_log#
uint8_t sl_btmesh_evt_config_client_heartbeat_pub_status_s::count_log
Heartbeat publication count logarithm-of-2 setting
Definition at line
8501
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
period_log#
uint8_t sl_btmesh_evt_config_client_heartbeat_pub_status_s::period_log
Heartbeat publication period logarithm-of-2 setting
Definition at line
8503
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
ttl#
uint8_t sl_btmesh_evt_config_client_heartbeat_pub_status_s::ttl
Time-to-live value for heartbeat messages
Definition at line
8505
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
features#
uint16_t sl_btmesh_evt_config_client_heartbeat_pub_status_s::features
Heartbeat trigger setting
Definition at line
8506
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h