Data structure of the lpn_polltimeout_status event.
Public Attribute Documentation#
result#
uint16_t sl_btmesh_evt_config_client_lpn_polltimeout_status_s::result
SL_STATUS_OK if successful. Error code otherwise.
Definition at line
8794
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
handle#
uint32_t sl_btmesh_evt_config_client_lpn_polltimeout_status_s::handle
Request handle
Definition at line
8796
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
poll_timeout_ms#
uint32_t sl_btmesh_evt_config_client_lpn_polltimeout_status_s::poll_timeout_ms
Poll timeout value, in milliseconds, for the specified LPN. The value reported is zero if the queried Friend does not have an ongoing friendship with the specified LPN.
Definition at line
8797
of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h