Data structure of the model_pub_status event.

Public Attributes#

uint16_t
uint32_t
uint16_t
uint16_t
uint8_t
uint32_t

Public Attribute Documentation#

result#

uint16_t sl_btmesh_evt_config_client_model_pub_status_s::result

SL_STATUS_OK if successful. Error code otherwise.


Definition at line 8375 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

handle#

uint32_t sl_btmesh_evt_config_client_model_pub_status_s::handle

Request handle


Definition at line 8377 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

address#

uint16_t sl_btmesh_evt_config_client_model_pub_status_s::address

The address to publish to. If this address is the unassigned address, the model is prevented from publishing. Note that, if state contains a Label UUID (full virtual address), the corresponding virtual address hash is returned in this parameter.


Definition at line 8378 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

appkey_index#

uint16_t sl_btmesh_evt_config_client_model_pub_status_s::appkey_index

The application key index used for the published messages


Definition at line 8385 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

credentials#

uint8_t sl_btmesh_evt_config_client_model_pub_status_s::credentials

Friendship credentials flag


Definition at line 8387 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

ttl#

uint8_t sl_btmesh_evt_config_client_model_pub_status_s::ttl

Publication time-to-live value


Definition at line 8388 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

period_ms#

uint32_t sl_btmesh_evt_config_client_model_pub_status_s::period_ms

Publication period in milliseconds


Definition at line 8389 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

retransmit_count#

uint8_t sl_btmesh_evt_config_client_model_pub_status_s::retransmit_count

Publication retransmission count


Definition at line 8390 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

retransmit_interval_ms#

uint16_t sl_btmesh_evt_config_client_model_pub_status_s::retransmit_interval_ms

Publication retransmission interval in milliseconds


Definition at line 8391 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h