GPIO - General Purpose Input/Output
Description
General Purpose Input/Output (GPIO) API.
This module contains functions to control the GPIO peripheral of Silicon Labs 32-bit MCUs and SoCs. The GPIO peripheral is used for pin configuration and direct pin manipulation and sensing as well as routing for peripheral pin connections.
Functions | |
void | GPIO_DbgLocationSet (unsigned int location) |
Sets the pin location of the debug pins (Serial Wire interface). | |
void | GPIO_ExtIntConfig (GPIO_Port_TypeDef port, unsigned int pin, unsigned int intNo, bool risingEdge, bool fallingEdge, bool enable) |
Configure the GPIO external pin interrupt. | |
void | GPIO_PinModeSet (GPIO_Port_TypeDef port, unsigned int pin, GPIO_Mode_TypeDef mode, unsigned int out) |
Set the mode for a GPIO pin. | |
GPIO_Mode_TypeDef | GPIO_PinModeGet (GPIO_Port_TypeDef port, unsigned int pin) |
Get the mode for a GPIO pin. | |
void | GPIO_EM4EnablePinWakeup (uint32_t pinmask, uint32_t polaritymask) |
Enable GPIO pin wake-up from EM4. | |
void | GPIO_DbgSWDClkEnable (bool enable) |
Enable/disable serial wire clock pin. | |
void | GPIO_DbgSWDIOEnable (bool enable) |
Enable/disable serial wire data I/O pin. | |
void | GPIO_DbgSWOEnable (bool enable) |
Enable/Disable serial wire output pin. | |
void | GPIO_EM4DisablePinWakeup (uint32_t pinmask) |
Disable GPIO pin wake-up from EM4. | |
uint32_t | GPIO_EM4GetPinWakeupCause (void) |
Check which GPIO pin(s) that caused a wake-up from EM4. | |
void | GPIO_EM4SetPinRetention (bool enable) |
Enable GPIO pin retention of output enable, output value, pull enable, and pull direction in EM4. | |
void | GPIO_InputSenseSet (uint32_t val, uint32_t mask) |
Enable/disable input sensing. | |
void | GPIO_IntClear (uint32_t flags) |
Clear one or more pending GPIO interrupts. | |
void | GPIO_IntDisable (uint32_t flags) |
Disable one or more GPIO interrupts. | |
void | GPIO_IntEnable (uint32_t flags) |
Enable one or more GPIO interrupts. | |
uint32_t | GPIO_IntGet (void) |
Get pending GPIO interrupts. | |
uint32_t | GPIO_IntGetEnabled (void) |
Get enabled and pending GPIO interrupt flags. | |
void | GPIO_IntSet (uint32_t flags) |
Set one or more pending GPIO interrupts from SW. | |
void | GPIO_Lock (void) |
Locks the GPIO configuration. | |
unsigned int | GPIO_PinInGet (GPIO_Port_TypeDef port, unsigned int pin) |
Read the pad value for a single pin in a GPIO port. | |
void | GPIO_PinOutClear (GPIO_Port_TypeDef port, unsigned int pin) |
Set a single pin in GPIO data out port register to 0. | |
unsigned int | GPIO_PinOutGet (GPIO_Port_TypeDef port, unsigned int pin) |
Get current setting for a pin in a GPIO port data out register. | |
void | GPIO_PinOutSet (GPIO_Port_TypeDef port, unsigned int pin) |
Set a single pin in GPIO data out register to 1. | |
void | GPIO_PinOutToggle (GPIO_Port_TypeDef port, unsigned int pin) |
Toggle a single pin in GPIO port data out register. | |
uint32_t | GPIO_PortInGet (GPIO_Port_TypeDef port) |
Read the pad values for GPIO port. | |
void | GPIO_PortOutClear (GPIO_Port_TypeDef port, uint32_t pins) |
Set bits in DOUT register for a port to 0. | |
uint32_t | GPIO_PortOutGet (GPIO_Port_TypeDef port) |
Get current setting for a GPIO port data out register. | |
void | GPIO_PortOutSet (GPIO_Port_TypeDef port, uint32_t pins) |
Set bits GPIO data out register to 1. | |
void | GPIO_PortOutSetVal (GPIO_Port_TypeDef port, uint32_t val, uint32_t mask) |
Set GPIO port data out register. | |
void | GPIO_PortOutToggle (GPIO_Port_TypeDef port, uint32_t pins) |
Toggle pins in GPIO port data out register. | |
void | GPIO_SlewrateSet (GPIO_Port_TypeDef port, uint32_t slewrate, uint32_t slewrateAlt) |
Set slewrate for pins on a GPIO port. | |
void | GPIO_Unlock (void) |
Unlocks the GPIO configuration. | |
void | GPIO_IntConfig (GPIO_Port_TypeDef port, unsigned int pin, bool risingEdge, bool fallingEdge, bool enable) |
Configure GPIO interrupt. | |
Enumerations | |
enum | GPIO_Port_TypeDef { gpioPortA = 0, gpioPortB = 1, gpioPortC = 2, gpioPortD = 3 } |
GPIO ports IDs. | |
enum | GPIO_Mode_TypeDef { gpioModeDisabled = _GPIO_P_MODEL_MODE0_DISABLED, gpioModeInput = _GPIO_P_MODEL_MODE0_INPUT, gpioModeInputPull = _GPIO_P_MODEL_MODE0_INPUTPULL, gpioModeInputPullFilter = _GPIO_P_MODEL_MODE0_INPUTPULLFILTER, gpioModePushPull = _GPIO_P_MODEL_MODE0_PUSHPULL, gpioModePushPullAlternate = _GPIO_P_MODEL_MODE0_PUSHPULLALT, gpioModeWiredOr = _GPIO_P_MODEL_MODE0_WIREDOR, gpioModeWiredOrPullDown = _GPIO_P_MODEL_MODE0_WIREDORPULLDOWN, gpioModeWiredAnd = _GPIO_P_MODEL_MODE0_WIREDAND, gpioModeWiredAndFilter = _GPIO_P_MODEL_MODE0_WIREDANDFILTER, gpioModeWiredAndPullUp = _GPIO_P_MODEL_MODE0_WIREDANDPULLUP, gpioModeWiredAndPullUpFilter = _GPIO_P_MODEL_MODE0_WIREDANDPULLUPFILTER, gpioModeWiredAndAlternate = _GPIO_P_MODEL_MODE0_WIREDANDALT, gpioModeWiredAndAlternateFilter = _GPIO_P_MODEL_MODE0_WIREDANDALTFILTER, gpioModeWiredAndAlternatePullUp = _GPIO_P_MODEL_MODE0_WIREDANDALTPULLUP, gpioModeWiredAndAlternatePullUpFilter = _GPIO_P_MODEL_MODE0_WIREDANDALTPULLUPFILTER } |
Pin mode. | |
Function Documentation
◆ GPIO_DbgLocationSet()
void GPIO_DbgLocationSet | ( | unsigned int | location | ) |
Sets the pin location of the debug pins (Serial Wire interface).
- Note
- Changing the pins used for debugging uncontrolled, may result in a lockout.
- Parameters
-
[in] location
The debug pin location to use (0-3).
◆ GPIO_ExtIntConfig()
void GPIO_ExtIntConfig | ( | GPIO_Port_TypeDef | port, |
unsigned int | pin, |
||
unsigned int | intNo, |
||
bool | risingEdge, |
||
bool | fallingEdge, |
||
bool | enable |
||
) |
Configure the GPIO external pin interrupt.
It is recommended to disable interrupts before configuring the GPIO pin interrupt. See GPIO_IntDisable() for more information.
The GPIO interrupt handler must be in place before enabling the interrupt.
Notice that any pending interrupt for the selected interrupt is cleared by this function.
- Note
- On series 0 devices, the pin number parameter is not used. The pin number used on these devices is hardwired to the interrupt with the same number.
On series 1 devices, the pin number can be selected freely within a group. Interrupt numbers are divided into 4 groups (intNo / 4) and valid pin number within the interrupt groups are: 0: pins 0-3 (interrupt number 0-3) 1: pins 4-7 (interrupt number 4-7) 2: pins 8-11 (interrupt number 8-11) 3: pins 12-15 (interrupt number 12-15)
- Parameters
-
[in] port
The port to associate with the pin
.[in] pin
The pin number on the port. [in] intNo
The interrupt number to trigger. [in] risingEdge
Set to true if the interrupt will be enabled on the rising edge. Otherwise, false. [in] fallingEdge
Set to true if the interrupt will be enabled on the falling edge. Otherwise, false. [in] enable
Set to true if the interrupt will be enabled after the configuration is complete. False to leave disabled. See GPIO_IntDisable() and GPIO_IntEnable().
◆ GPIO_PinModeSet()
void GPIO_PinModeSet | ( | GPIO_Port_TypeDef | port, |
unsigned int | pin, |
||
GPIO_Mode_TypeDef | mode, |
||
unsigned int | out |
||
) |
Set the mode for a GPIO pin.
- Parameters
-
[in] port
The GPIO port to access. [in] pin
The pin number in the port. [in] mode
The desired pin mode. [in] out
A value to set for the pin in the DOUT register. The DOUT setting is important for some input mode configurations to determine the pull-up/down direction.
◆ GPIO_PinModeGet()
GPIO_Mode_TypeDef GPIO_PinModeGet | ( | GPIO_Port_TypeDef | port, |
unsigned int | pin |
||
) |
Get the mode for a GPIO pin.
- Parameters
-
[in] port
The GPIO port to access. [in] pin
The pin number in the port.
- Returns
- The pin mode.
◆ GPIO_EM4EnablePinWakeup()
void GPIO_EM4EnablePinWakeup | ( | uint32_t | pinmask, |
uint32_t | polaritymask |
||
) |
Enable GPIO pin wake-up from EM4.
When the function exits, EM4 mode can be safely entered.
- Note
- It is assumed that the GPIO pin modes are set correctly. Valid modes are gpioModeInput and gpioModeInputPull.
- Parameters
-
[in] pinmask
A bitmask containing the bitwise logic OR of which GPIO pin(s) to enable. See Reference Manuals for a pinmask to the GPIO port/pin mapping. [in] polaritymask
A bitmask containing the bitwise logic OR of GPIO pin(s) wake-up polarity. See Reference Manuals for pinmask-to-GPIO port/pin mapping.
◆ GPIO_DbgSWDClkEnable()
|
inline |
Enable/disable serial wire clock pin.
- Note
- Disabling SWDClk will disable the debug interface, which may result in a lockout if done early in startup (before debugger is able to halt core).
- Parameters
-
[in] enable
- false - disable serial wire clock.
- true - enable serial wire clock (default after reset).
◆ GPIO_DbgSWDIOEnable()
|
inline |
Enable/disable serial wire data I/O pin.
- Note
- Disabling SWDClk will disable the debug interface, which may result in a lockout if done early in startup (before debugger is able to halt core).
- Parameters
-
[in] enable
- false - disable serial wire data pin.
- true - enable serial wire data pin (default after reset).
◆ GPIO_DbgSWOEnable()
|
inline |
Enable/Disable serial wire output pin.
- Note
- Enabling this pin is not sufficient to fully enable serial wire output, which is also dependent on issues outside the GPIO module. Refer to DBG_SWOEnable().
- Parameters
-
[in] enable
- false - disable serial wire viewer pin (default after reset).
- true - enable serial wire viewer pin.
◆ GPIO_EM4DisablePinWakeup()
|
inline |
Disable GPIO pin wake-up from EM4.
- Parameters
-
[in] pinmask
Bit mask containing the bitwise logic OR of which GPIO pin(s) to disable. Refer to Reference Manuals for pinmask to GPIO port/pin mapping.
◆ GPIO_EM4GetPinWakeupCause()
|
inline |
Check which GPIO pin(s) that caused a wake-up from EM4.
- Returns
- Bit mask containing the bitwise logic OR of which GPIO pin(s) caused the wake-up. Refer to Reference Manuals for pinmask to GPIO port/pin mapping.
◆ GPIO_EM4SetPinRetention()
|
inline |
Enable GPIO pin retention of output enable, output value, pull enable, and pull direction in EM4.
- Note
- On series 0 devices EM4 gpio retention can either be turned on or off. On series 1 devices there are three EM4 GPIO retention modes available. These modes are "Disabled", "EM4EXIT" and "SWUNLATCH". Use the EMU_EM4Init() to configure the GPIO retention mode on a series 1 device.
The behavior of this function depends on the configured GPIO retention mode. If the GPIO retention mode is configured to be "SWUNLATCH" then this function will not change anything. If the retention mode is anything else then this function will set the GPIO retention mode to "EM4EXIT" when the enable argument is true, and "Disabled" when false.
- Parameters
-
[in] enable
- true - enable EM4 pin retention.
- false - disable EM4 pin retention.
◆ GPIO_InputSenseSet()
|
inline |
Enable/disable input sensing.
Disabling input sensing if not used, can save some energy consumption.
- Parameters
-
[in] val
Bitwise logic OR of one or more of: - GPIO_INSENSE_INT - interrupt input sensing.
- GPIO_INSENSE_PRS - peripheral reflex system input sensing.
[in] mask
Mask containing bitwise logic OR of bits similar as for val
used to indicate which input sense options to disable/enable.
◆ GPIO_IntClear()
|
inline |
Clear one or more pending GPIO interrupts.
- Parameters
-
[in] flags
Bitwise logic OR of GPIO interrupt sources to clear.
◆ GPIO_IntDisable()
|
inline |
Disable one or more GPIO interrupts.
- Parameters
-
[in] flags
GPIO interrupt sources to disable.
◆ GPIO_IntEnable()
|
inline |
Enable one or more GPIO interrupts.
- Note
- Depending on the use, a pending interrupt may already be set prior to enabling the interrupt. To ignore a pending interrupt, consider using GPIO_IntClear() prior to enabling the interrupt.
- Parameters
-
[in] flags
GPIO interrupt sources to enable.
◆ GPIO_IntGet()
|
inline |
Get pending GPIO interrupts.
- Returns
- GPIO interrupt sources pending.
◆ GPIO_IntGetEnabled()
|
inline |
Get enabled and pending GPIO interrupt flags.
Useful for handling more interrupt sources in the same interrupt handler.
- Note
- Interrupt flags are not cleared by the use of this function.
- Returns
- Pending and enabled GPIO interrupt sources. The return value is the bitwise AND combination of
- the OR combination of enabled interrupt sources in GPIO_IEN register and
- the OR combination of valid interrupt flags in GPIO_IF register.
◆ GPIO_IntSet()
|
inline |
Set one or more pending GPIO interrupts from SW.
- Parameters
-
[in] flags
GPIO interrupt sources to set to pending.
◆ GPIO_Lock()
|
inline |
Locks the GPIO configuration.
◆ GPIO_PinInGet()
|
inline |
Read the pad value for a single pin in a GPIO port.
- Parameters
-
[in] port
The GPIO port to access. [in] pin
The pin number to read.
- Returns
- The pin value, 0 or 1.
◆ GPIO_PinOutClear()
|
inline |
Set a single pin in GPIO data out port register to 0.
- Note
- In order for the setting to take effect on the output pad, the pin must have been configured properly. If not, it will take effect whenever the pin has been properly configured.
- Parameters
-
[in] port
The GPIO port to access. [in] pin
The pin to set.
◆ GPIO_PinOutGet()
|
inline |
Get current setting for a pin in a GPIO port data out register.
- Parameters
-
[in] port
The GPIO port to access. [in] pin
The pin to get setting for.
- Returns
- The DOUT setting for the requested pin, 0 or 1.
◆ GPIO_PinOutSet()
|
inline |
Set a single pin in GPIO data out register to 1.
- Note
- In order for the setting to take effect on the output pad, the pin must have been configured properly. If not, it will take effect whenever the pin has been properly configured.
- Parameters
-
[in] port
The GPIO port to access. [in] pin
The pin to set.
◆ GPIO_PinOutToggle()
|
inline |
Toggle a single pin in GPIO port data out register.
- Note
- In order for the setting to take effect on the output pad, the pin must have been configured properly. If not, it will take effect whenever the pin has been properly configured.
- Parameters
-
[in] port
The GPIO port to access. [in] pin
The pin to toggle.
◆ GPIO_PortInGet()
|
inline |
Read the pad values for GPIO port.
- Parameters
-
[in] port
The GPIO port to access.
- Returns
- The pad values for the GPIO port.
◆ GPIO_PortOutClear()
|
inline |
Set bits in DOUT register for a port to 0.
- Note
- In order for the setting to take effect on the output pad, the pin must have been configured properly. If not, it will take effect whenever the pin has been properly configured.
- Parameters
-
[in] port
The GPIO port to access. [in] pins
Bit mask for bits to clear in DOUT register.
◆ GPIO_PortOutGet()
|
inline |
Get current setting for a GPIO port data out register.
- Parameters
-
[in] port
The GPIO port to access.
- Returns
- The data out setting for the requested port.
◆ GPIO_PortOutSet()
|
inline |
Set bits GPIO data out register to 1.
- Note
- In order for the setting to take effect on the respective output pads, the pins must have been configured properly. If not, it will take effect whenever the pin has been properly configured.
- Parameters
-
[in] port
The GPIO port to access. [in] pins
Bit mask for bits to set to 1 in DOUT register.
◆ GPIO_PortOutSetVal()
|
inline |
Set GPIO port data out register.
- Note
- In order for the setting to take effect on the respective output pads, the pins must have been configured properly. If not, it will take effect whenever the pin has been properly configured.
- Parameters
-
[in] port
The GPIO port to access. [in] val
Value to write to port data out register. [in] mask
Mask indicating which bits to modify.
◆ GPIO_PortOutToggle()
|
inline |
Toggle pins in GPIO port data out register.
- Note
- In order for the setting to take effect on the output pad, the pin must have been configured properly. If not, it will take effect whenever the pin has been properly configured.
- Parameters
-
[in] port
The GPIO port to access. [in] pins
Bit mask with pins to toggle.
◆ GPIO_SlewrateSet()
|
inline |
Set slewrate for pins on a GPIO port.
- Parameters
-
[in] port
The GPIO port to configure. [in] slewrate
The slewrate to configure for pins on this GPIO port. [in] slewrateAlt
The slewrate to configure for pins using alternate modes on this GPIO port.
◆ GPIO_Unlock()
|
inline |
Unlocks the GPIO configuration.
◆ GPIO_IntConfig()
|
inline |
Configure GPIO interrupt.
If reconfiguring a GPIO interrupt that is already enabled, it is generally recommended to disable it first, see GPIO_IntDisable().
The actual GPIO interrupt handler must be in place before enabling the interrupt.
Notice that any pending interrupt for the selected pin is cleared by this function.
- Note
- A certain pin number can only be associated with one port; i.e., if GPIO interrupt 1 is assigned to port A/pin 1, then it is not possible to use pin 1 from any other ports for interrupts. Refer to the reference manual. On devices which implement GPIO_EXTIPINSEL registers a more flexible approach is possible, refer to GPIO_ExtIntConfig().
- Parameters
-
[in] port
The port to associate with pin
.[in] pin
The pin number on the port ( == GPIO EXTI interrupt number). [in] risingEdge
Set to true if interrupts will be enabled on rising edge, otherwise false. [in] fallingEdge
Set to true if interrupts will be enabled on falling edge, otherwise false. [in] enable
Set to true if interrupt will be enabled after configuration completed, false to leave disabled. See GPIO_IntDisable() and GPIO_IntEnable().
Enumeration Type Documentation
◆ GPIO_Port_TypeDef
enum GPIO_Port_TypeDef |
◆ GPIO_Mode_TypeDef
enum GPIO_Mode_TypeDef |
Pin mode.
For more details on each mode, refer to the reference manual.