MSC_EccConfig_TypeDef Struct Reference
ECC configuration.
#include <em_msc.h>
Data Fields | |
bool | enableEccBank [MSC_ECC_BANKS] |
Array of bools to enable/disable Error Correcting Code (ECC) for each RAM bank that supports ECC on the device. | |
uint32_t | dmaChannels [2] |
Array of 2 DMA channel numbers to use for ECC initialization. | |
ECC configuration.
Field Documentation
◆ enableEccBank
bool MSC_EccConfig_TypeDef::enableEccBank[MSC_ECC_BANKS] |
Array of bools to enable/disable Error Correcting Code (ECC) for each RAM bank that supports ECC on the device.
◆ dmaChannels
uint32_t MSC_EccConfig_TypeDef::dmaChannels[2] |
Array of 2 DMA channel numbers to use for ECC initialization.