RTCDRVEMDRV
Detailed Description
Real-time Clock Driver.
The source files for the RTCDRV device driver library resides in the emdrv/rtcdrv folder, and are named rtcdriver.c and rtcdriver.h .
Introduction
The RTCDRV driver use the RTC peripheral of a device in Silicon Laboratories Gecko microcontroller family to provide a user configurable number of software millisecond timers. Two kinds of timers are supported; oneshot timers and periodic timers. Timers will, when their timeout period has expired, call a user supplied callback function.
- Note
- The callback function is called from within an interrupt handler with interrupts disabled.
In addition to the timers, RTCDRV also offers an optional wallclock functionality. The wallclock keeps track of the number of seconds elapsed since RTCDRV was initialized.
RTCDRV resolution is 1 ms with 244 us accuracy. On the EFM32G family (classic Gecko's) the accuracy is 61 us. Since RTCDRV is interrupt driven using the default RTC interrupt priority level, timeout accuracy will be affected by the interrupt latency of the system.
Configuration Options
Some properties of the RTCDRV driver are compile-time configurable. These properties are stored in a file named rtcdrv_config.h. A template for this file, containing default values, resides in the emdrv/config folder. Currently the configuration options are:
- The number of timers that RTCDRV provides.
- Inclusion of the wallclock functionality.
- Integration with SLEEP driver.
When integration with the SLEEP driver is enabled, RTCDRV will keep the SLEEP driver updated with regards to which energy mode that can be safely used.
To configure RTCDRV, provide your own configuration file. Here is a sample rtcdrv_config.h file:
#ifndef SILICON_LABS_RTCDRV_CONFIG_H #define SILICON_LABS_RTCDRV_CONFIG_H // Define how many timers RTCDRV provide. #define EMDRV_RTCDRV_NUM_TIMERS (4) // Uncomment the following line to include wallclock functionality. //#define EMDRV_RTCDRV_WALLCLOCK_CONFIG // Uncomment the following line to enable integration with SLEEP driver. //#define EMDRV_RTCDRV_SLEEPDRV_INTEGRATION // Uncomment one of the following lines to let RTCDRV clock on LFRCO or PLFRCO, // the default is LFXO. //#define EMDRV_RTCDRV_USE_LFRCO //#define EMDRV_RTCDRV_USE_PLFRCO #endif
The API
This section contain brief descriptions of the functions in the API. You will find detailed information on input and output parameters and return values by clicking on the hyperlinked function names. Most functions return an error code, ECODE_EMDRV_RTCDRV_OK is returned on success, see ecode.h and rtcdriver.h for other error codes.
Your application code must include one header file: rtcdriver.h .
All functions defined in the API can be called from within interrupt handlers.
RTCDRV_Init()
,
RTCDRV_DeInit()
These functions initializes or deinitializes the RTCDRV driver. Typically RTCDRV_Init() is called once in your startup code.
RTCDRV_StartTimer()
,
RTCDRV_StopTimer()
Start/Stop a timer. When a timer expire, a user supplied callback function is called. A pointer to this function is passed to RTCDRV_StartTimer(). Refer to
TimerCallback
for details of the callback prototype. Note that it is legal to start an already started timer, it will then just be restarted with the new timeout value.
RTCDRV_AllocateTimer()
,
RTCDRV_FreeTimer()
Reserve/release a timer. Many functions in the API require a timer ID as input parameter. Use RTCDRV_AllocateTimer() to aquire such a reference.
RTCDRV_TimeRemaining()
Get time left to timer expiry.
RTCDRV_Delay()
Millisecond delay function. This is an "active wait" delay function.
RTCDRV_IsRunning()
Check if a timer is running.
RTCDRV_GetWallClock()
,
RTCDRV_SetWallClock()
Get or set wallclock time.
RTCDRV_GetWallClockTicks32()
,
RTCDRV_GetWallClockTicks64()
Get wallclock time expressed as number of RTC/RTCC counter ticks, available both as 32bit and 64 bit values.
RTCDRV_MsecsToTicks()
,
RTCDRV_SecsToTicks()
,
RTCDRV_TicksToMsec()
,
RTCDRV_TicksToSec()
Conversion functions between seconds, milliseconds and RTC/RTCC counter ticks.
The timer expiry callback function:
The callback function, prototyped as
RTCDRV_Callback_t()
, is called from within the RTC peripheral interrupt handler on timer expiry. RTCDRV_Callback_t( RTCDRV_TimerID_t id ) is called with the timer id as input parameter.
The timer type:
Timers are either of oneshot type or of periodic type.
- Oneshot timer run only once toward their expiry.
- Periodic timers will be automatically restartet when they expire.
The timer type is an enumeration, see RTCDRV_TimerType_t for details.
Example
#include "rtcdriver.h" #include <stddef.h> int i = 0; RTCDRV_TimerID_t id; void myCallback( RTCDRV_TimerID_t id, void * user ) { (void) user; // unused argument in this example i++; if ( i < 10 ) { // Restart timer RTCDRV_StartTimer( id, rtcdrvTimerTypeOneshot, 100, myCallback, NULL ); } } int main( void ) { // Initialization of RTCDRV driver RTCDRV_Init(); // Reserve a timer RTCDRV_AllocateTimer( &id ); // Start a oneshot timer with 100 millisecond timeout RTCDRV_StartTimer( id, rtcdrvTimerTypeOneshot, 100, myCallback, NULL ); return 0; }
Macros |
|
#define | ECODE_EMDRV_RTCDRV_ALL_TIMERS_USED ( ECODE_EMDRV_RTCDRV_BASE | 0x00000001) |
No timers available.
|
|
#define | ECODE_EMDRV_RTCDRV_ILLEGAL_TIMER_ID ( ECODE_EMDRV_RTCDRV_BASE | 0x00000002) |
Illegal timer id.
|
|
#define | ECODE_EMDRV_RTCDRV_OK ( ECODE_OK ) |
Success return value.
|
|
#define | ECODE_EMDRV_RTCDRV_PARAM_ERROR ( ECODE_EMDRV_RTCDRV_BASE | 0x00000004) |
Illegal input parameter.
|
|
#define | ECODE_EMDRV_RTCDRV_TIMER_NOT_ALLOCATED ( ECODE_EMDRV_RTCDRV_BASE | 0x00000003) |
Timer is not allocated.
|
|
#define | ECODE_EMDRV_RTCDRV_TIMER_NOT_RUNNING ( ECODE_EMDRV_RTCDRV_BASE | 0x00000005) |
Timer is not running.
|
|
Typedefs |
|
typedef void(* | RTCDRV_Callback_t ) ( RTCDRV_TimerID_t id, void *user) |
Typedef for the user supplied callback function which is called when a timer elapse.
|
|
typedef uint32_t | RTCDRV_TimerID_t |
Timer ID.
|
|
Enumerations |
|
enum |
RTCDRV_TimerType_t
{
rtcdrvTimerTypeOneshot = 0, rtcdrvTimerTypePeriodic = 1 } |
Timer type enumerator.
|
|
Functions |
|
Ecode_t | RTCDRV_AllocateTimer ( RTCDRV_TimerID_t *id) |
Allocate timer.
|
|
Ecode_t | RTCDRV_DeInit (void) |
Deinitialize RTCDRV driver.
|
|
Ecode_t | RTCDRV_Delay (uint32_t ms) |
Millisecond delay function.
|
|
Ecode_t | RTCDRV_FreeTimer ( RTCDRV_TimerID_t id) |
Free timer.
|
|
uint32_t | RTCDRV_GetWallClock (void) |
Get wallclock time.
|
|
uint32_t | RTCDRV_GetWallClockTicks32 (void) |
Get wallclock tick count as a 32bit value. At 4 ticks per millisecond, overflow occurs after approximately 12.5 days.
|
|
uint64_t | RTCDRV_GetWallClockTicks64 (void) |
Get wallclock tick count as a 64 bit value. This will never overflow.
|
|
Ecode_t | RTCDRV_Init (void) |
Initialize RTCDRV driver.
|
|
Ecode_t | RTCDRV_IsRunning ( RTCDRV_TimerID_t id, bool *isRunning) |
Check if a given timer is running.
|
|
uint64_t | RTCDRV_MsecsToTicks (uint32_t ms) |
Convert from milliseconds to RTC/RTCC ticks.
|
|
uint64_t | RTCDRV_SecsToTicks (uint32_t secs) |
Convert from seconds to RTC/RTCC ticks.
|
|
Ecode_t | RTCDRV_SetWallClock (uint32_t secs) |
Set wallclock time.
|
|
Ecode_t | RTCDRV_StartTimer ( RTCDRV_TimerID_t id, RTCDRV_TimerType_t type, uint32_t timeout, RTCDRV_Callback_t callback, void *user) |
Start a timer.
|
|
Ecode_t | RTCDRV_StopTimer ( RTCDRV_TimerID_t id) |
Stop a given timer.
|
|
uint32_t | RTCDRV_TicksToMsec (uint64_t ticks) |
Convert from RTC/RTCC ticks to milliseconds.
|
|
uint32_t | RTCDRV_TicksToSec (uint64_t ticks) |
Convert from RTC/RTCC ticks to seconds.
|
|
Ecode_t | RTCDRV_TimeRemaining ( RTCDRV_TimerID_t id, uint32_t *timeRemaining) |
Get time left before a given timer expires.
|
|
Typedef Documentation
typedef void(* RTCDRV_Callback_t) ( RTCDRV_TimerID_t id, void *user) |
Typedef for the user supplied callback function which is called when a timer elapse.
- Note
- This callback is called from within an interrupt handler with interrupts disabled.
- Parameters
-
[in] id
The timer id. [in] user
Extra parameter for user application.
Definition at line
63
of file
rtcdriver.h
.
Enumeration Type Documentation
enum RTCDRV_TimerType_t |
Function Documentation
Ecode_t RTCDRV_AllocateTimer | ( | RTCDRV_TimerID_t * |
id
|
) |
Allocate timer.
Reserve a timer instance.
- Parameters
-
[out] id
The id of the reserved timer.
- Returns
-
ECODE_EMDRV_RTCDRV_OK
on success.
ECODE_EMDRV_RTCDRV_ALL_TIMERS_USED when no timers are available.
ECODE_EMDRV_RTCDRV_PARAM_ERROR if an invalid id pointer was supplied.
Definition at line
232
of file
rtcdriver.c
.
References CORE_DECLARE_IRQ_STATE , CORE_ENTER_ATOMIC , CORE_EXIT_ATOMIC , ECODE_EMDRV_RTCDRV_ALL_TIMERS_USED , ECODE_EMDRV_RTCDRV_OK , and ECODE_EMDRV_RTCDRV_PARAM_ERROR .
Referenced by SPIDRV_Init() , and UTIL_sleepInit() .
Ecode_t RTCDRV_DeInit | ( | void |
|
) |
Deinitialize RTCDRV driver.
Will disable interrupts and turn off the clock to the underlying hardware timer. If integration with SLEEP module is enabled it will remove any restriction that are set on energy mode usage.
- Returns
- ECODE_EMDRV_RTCDRV_OK .
Definition at line
418
of file
rtcdriver.c
.
References CMU_ClockEnable() , cmuClock_RTC , ECODE_EMDRV_RTCDRV_OK , RTC_Enable() , SLEEP_SleepBlockEnd() , and sleepEM3 .
Ecode_t RTCDRV_Delay | ( | uint32_t |
ms
|
) |
Millisecond delay function.
- Parameters
-
[in] ms
Milliseconds to stay in the delay function.
- Returns
- ECODE_EMDRV_RTCDRV_OK .
Definition at line
271
of file
rtcdriver.c
.
References ECODE_EMDRV_RTCDRV_OK .
Referenced by delay_10ms() , and delay_1ms() .
Ecode_t RTCDRV_FreeTimer | ( | RTCDRV_TimerID_t |
id
|
) |
Free timer.
Release a reserved timer.
- Parameters
-
[out] id
The id of the timer to release.
- Returns
-
ECODE_EMDRV_RTCDRV_OK
on success.
ECODE_EMDRV_RTCDRV_ILLEGAL_TIMER_ID if id has an illegal value.
Definition at line
299
of file
rtcdriver.c
.
References CORE_ATOMIC_SECTION , ECODE_EMDRV_RTCDRV_ILLEGAL_TIMER_ID , and ECODE_EMDRV_RTCDRV_OK .
Referenced by SPIDRV_DeInit() .
uint32_t RTCDRV_GetWallClock | ( | void |
|
) |
Get wallclock time.
- Returns
- Seconds elapsed since RTCDRV was initialized.
Definition at line
759
of file
rtcdriver.c
.
References RTCDRV_GetWallClockTicks32() .
uint32_t RTCDRV_GetWallClockTicks32 | ( | void |
|
) |
Get wallclock tick count as a 32bit value. At 4 ticks per millisecond, overflow occurs after approximately 12.5 days.
- Returns
- Wallclock tick counter.
Definition at line
775
of file
rtcdriver.c
.
Referenced by RTCDRV_GetWallClock() , and RTCDRV_SetWallClock() .
uint64_t RTCDRV_GetWallClockTicks64 | ( | void |
|
) |
Get wallclock tick count as a 64 bit value. This will never overflow.
- Returns
- Wallclock tick counter.
Definition at line
801
of file
rtcdriver.c
.
Ecode_t RTCDRV_Init | ( | void |
|
) |
Initialize RTCDRV driver.
Will enable all necessary clocks. Initializes internal datastructures and configures the underlying hardware timer.
- Returns
- ECODE_EMDRV_RTCDRV_OK .
Definition at line
325
of file
rtcdriver.c
.
References CMU_ClockDivSet() , CMU_ClockEnable() , CMU_ClockSelectSet() , CMU_DivToLog2() , cmuClock_LFA , cmuClock_RTC , ECODE_EMDRV_RTCDRV_OK , RTC_Init() , SLEEP_SleepBlockBegin() , and sleepEM3 .
Referenced by SPIDRV_Init() , and UTIL_sleepInit() .
Ecode_t RTCDRV_IsRunning | ( | RTCDRV_TimerID_t |
id,
|
bool * |
isRunning
|
||
) |
Check if a given timer is running.
- Parameters
-
[in] id
The id of the timer to query. [out] isRunning
True if timer is running. False if not running. Only valid if return status is ECODE_EMDRV_RTCDRV_OK.
- Returns
-
ECODE_EMDRV_RTCDRV_OK
on success.
ECODE_EMDRV_RTCDRV_ILLEGAL_TIMER_ID if id has an illegal value.
ECODE_EMDRV_RTCDRV_TIMER_NOT_ALLOCATED if the timer is not reserved.
ECODE_EMDRV_RTCDRV_PARAM_ERROR if an invalid isRunning pointer was supplied.
Definition at line
469
of file
rtcdriver.c
.
References CORE_DECLARE_IRQ_STATE , CORE_ENTER_ATOMIC , CORE_EXIT_ATOMIC , ECODE_EMDRV_RTCDRV_ILLEGAL_TIMER_ID , ECODE_EMDRV_RTCDRV_OK , ECODE_EMDRV_RTCDRV_PARAM_ERROR , and ECODE_EMDRV_RTCDRV_TIMER_NOT_ALLOCATED .
uint64_t RTCDRV_MsecsToTicks | ( | uint32_t |
ms
|
) |
Convert from milliseconds to RTC/RTCC ticks.
- Parameters
-
[in] ms
Millisecond value to convert.
- Returns
- Number of ticks.
Definition at line
842
of file
rtcdriver.c
.
uint64_t RTCDRV_SecsToTicks | ( | uint32_t |
secs
|
) |
Convert from seconds to RTC/RTCC ticks.
- Parameters
-
[in] secs
Second value to convert.
- Returns
- Number of ticks.
Definition at line
858
of file
rtcdriver.c
.
Ecode_t RTCDRV_SetWallClock | ( | uint32_t |
secs
|
) |
Set wallclock time.
- Parameters
-
[in] secs
Value to set (seconds).
- Returns
- ECODE_EMDRV_RTCDRV_OK
Definition at line
825
of file
rtcdriver.c
.
References ECODE_EMDRV_RTCDRV_OK , and RTCDRV_GetWallClockTicks32() .
Ecode_t RTCDRV_StartTimer | ( | RTCDRV_TimerID_t |
id,
|
RTCDRV_TimerType_t |
type,
|
||
uint32_t |
timeout,
|
||
RTCDRV_Callback_t |
callback,
|
||
void * |
user
|
||
) |
Start a timer.
- Note
- It is legal to start an already running timer.
- Parameters
-
[in] id
The id of the timer to start. [in] type
Timer type, oneshot or periodic. See RTCDRV_TimerType_t . [in] timeout
Timeout expressed in milliseconds. If the timeout value is 0, the callback function will be called immediately and the timer will not be started. [in] callback
Function to call on timer expiry. See RTCDRV_Callback_t . NULL is a legal value. [in] user
Extra callback function parameter for user application.
- Returns
-
ECODE_EMDRV_RTCDRV_OK
on success.
ECODE_EMDRV_RTCDRV_ILLEGAL_TIMER_ID if id has an illegal value.
ECODE_EMDRV_RTCDRV_TIMER_NOT_ALLOCATED if the timer is not reserved.
Definition at line
516
of file
rtcdriver.c
.
References CORE_DECLARE_IRQ_STATE , CORE_ENTER_ATOMIC , CORE_EXIT_ATOMIC , ECODE_EMDRV_RTCDRV_ILLEGAL_TIMER_ID , ECODE_EMDRV_RTCDRV_OK , ECODE_EMDRV_RTCDRV_TIMER_NOT_ALLOCATED , rtcdrvTimerTypePeriodic , SL_MIN , SLEEP_SleepBlockBegin() , and sleepEM3 .
Referenced by SPIDRV_SReceive() , SPIDRV_SReceiveB() , SPIDRV_STransfer() , SPIDRV_STransferB() , SPIDRV_STransmit() , SPIDRV_STransmitB() , UTIL_sleep() , and UTIL_waitForEvent() .
Ecode_t RTCDRV_StopTimer | ( | RTCDRV_TimerID_t |
id
|
) |
Stop a given timer.
- Parameters
-
[in] id
The id of the timer to stop.
- Returns
-
ECODE_EMDRV_RTCDRV_OK
on success.
ECODE_EMDRV_RTCDRV_ILLEGAL_TIMER_ID if id has an illegal value.
ECODE_EMDRV_RTCDRV_TIMER_NOT_ALLOCATED if the timer is not reserved.
Definition at line
666
of file
rtcdriver.c
.
References CORE_DECLARE_IRQ_STATE , CORE_ENTER_ATOMIC , CORE_EXIT_ATOMIC , ECODE_EMDRV_RTCDRV_ILLEGAL_TIMER_ID , ECODE_EMDRV_RTCDRV_OK , and ECODE_EMDRV_RTCDRV_TIMER_NOT_ALLOCATED .
Referenced by SPIDRV_AbortTransfer() , and SPIDRV_DeInit() .
uint32_t RTCDRV_TicksToMsec | ( | uint64_t |
ticks
|
) |
Convert from RTC/RTCC ticks to milliseconds.
- Parameters
-
[in] ticks
Number of ticks to convert.
- Returns
- Number of milliseconds.
Definition at line
874
of file
rtcdriver.c
.
uint32_t RTCDRV_TicksToSec | ( | uint64_t |
ticks
|
) |
Convert from RTC/RTCC ticks to seconds.
- Parameters
-
[in] ticks
Number of ticks to convert.
- Returns
- Number of seconds.
Definition at line
890
of file
rtcdriver.c
.
Ecode_t RTCDRV_TimeRemaining | ( | RTCDRV_TimerID_t |
id,
|
uint32_t * |
timeRemaining
|
||
) |
Get time left before a given timer expires.
- Parameters
-
[in] id
The id of the timer to query. [out] timeRemaining
Time left expressed in milliseconds. Only valid if return status is ECODE_EMDRV_RTCDRV_OK.
- Returns
-
ECODE_EMDRV_RTCDRV_OK
on success.
ECODE_EMDRV_RTCDRV_ILLEGAL_TIMER_ID if id has an illegal value.
ECODE_EMDRV_RTCDRV_TIMER_NOT_ALLOCATED if the timer is not reserved.
ECODE_EMDRV_RTCDRV_TIMER_NOT_RUNNING if the timer is not running.
ECODE_EMDRV_RTCDRV_PARAM_ERROR if an invalid timeRemaining pointer was supplied.
Definition at line
703
of file
rtcdriver.c
.
References CORE_DECLARE_IRQ_STATE , CORE_ENTER_ATOMIC , CORE_EXIT_ATOMIC , ECODE_EMDRV_RTCDRV_ILLEGAL_TIMER_ID , ECODE_EMDRV_RTCDRV_OK , ECODE_EMDRV_RTCDRV_PARAM_ERROR , ECODE_EMDRV_RTCDRV_TIMER_NOT_ALLOCATED , and ECODE_EMDRV_RTCDRV_TIMER_NOT_RUNNING .
Referenced by UTIL_waitForEvent() .