ACMP_CapsenseInit_TypeDef Struct ReferenceEMLIB > ACMP

Capsense initialization structure.

Definition at line 525 of file em_acmp.h .

#include < em_acmp.h >

Data Fields

uint32_t biasProg
bool enable
bool fullBias
bool halfBias
ACMP_HysteresisLevel_TypeDef hysteresisLevel
bool lowPowerReferenceEnabled
ACMP_CapsenseResistor_TypeDef resistor
uint32_t vddLevel
ACMP_WarmTime_TypeDef warmTime

Field Documentation

uint32_t ACMP_CapsenseInit_TypeDef::biasProg

Bias current. See the ACMP chapter about bias and response time in the reference manual for details.

Definition at line 538 of file em_acmp.h .

Referenced by ACMP_CapsenseInit() .

bool ACMP_CapsenseInit_TypeDef::enable

If true, ACMP is being enabled after configuration.

Definition at line 592 of file em_acmp.h .

Referenced by ACMP_CapsenseInit() .

bool ACMP_CapsenseInit_TypeDef::fullBias

Full bias current. See the ACMP chapter about bias and response time in the reference manual for details.

Definition at line 528 of file em_acmp.h .

Referenced by ACMP_CapsenseInit() , and CAPLESENSE_setupACMP() .

bool ACMP_CapsenseInit_TypeDef::halfBias

Half bias current. See the ACMP chapter about bias and response time in the reference manual for details.

Definition at line 533 of file em_acmp.h .

Referenced by ACMP_CapsenseInit() .

ACMP_HysteresisLevel_TypeDef ACMP_CapsenseInit_TypeDef::hysteresisLevel

Hysteresis level

Definition at line 548 of file em_acmp.h .

Referenced by ACMP_CapsenseInit() .

bool ACMP_CapsenseInit_TypeDef::lowPowerReferenceEnabled

Low power reference enabled. This setting, if enabled, reduces the power used by the VDD and bandgap references.

Definition at line 564 of file em_acmp.h .

Referenced by ACMP_CapsenseInit() .

ACMP_CapsenseResistor_TypeDef ACMP_CapsenseInit_TypeDef::resistor

Resistor used in the capacative sensing circuit. For values see your device datasheet.

Definition at line 559 of file em_acmp.h .

Referenced by ACMP_CapsenseInit() .

uint32_t ACMP_CapsenseInit_TypeDef::vddLevel

Vdd reference value. VDD_SCALED = (Vdd * VDDLEVEL) / 63. Valid values are in the range 0-63.

Definition at line 570 of file em_acmp.h .

Referenced by ACMP_CapsenseInit() .

ACMP_WarmTime_TypeDef ACMP_CapsenseInit_TypeDef::warmTime

Warmup time. This is measured in HFPERCLK cycles and should be about 10us in wall clock time.

Definition at line 543 of file em_acmp.h .

Referenced by ACMP_CapsenseInit() .


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/emlib/inc/ em_acmp.h