ADC_InitScan_TypeDef Struct ReferenceEMLIB > ADC

Scan sequence init structure.

Definition at line 862 of file em_adc.h .

#include < em_adc.h >

Data Fields

ADC_AcqTime_TypeDef acqTime
bool diff
uint32_t input
bool leftAdjust
bool prsEnable
ADC_PRSSEL_TypeDef prsSel
ADC_Ref_TypeDef reference
bool rep
ADC_Res_TypeDef resolution

Field Documentation

ADC_AcqTime_TypeDef ADC_InitScan_TypeDef::acqTime

Acquisition time (in ADC clock cycles).

Definition at line 870 of file em_adc.h .

Referenced by ADC_InitScan() .

bool ADC_InitScan_TypeDef::diff

Select if single ended or differential input.

Definition at line 900 of file em_adc.h .

Referenced by ADC_InitScan() .

uint32_t ADC_InitScan_TypeDef::input

Scan input selection. If single ended ( diff is false), use logical combination of ADC_SCANCTRL_INPUTMASK_CHx defines. If differential input ( diff is true), use logical combination of ADC_SCANCTRL_INPUTMASK_CHxCHy defines. (Notice underscore prefix for defines used.)

Definition at line 888 of file em_adc.h .

Referenced by ADC_InitScan() .

bool ADC_InitScan_TypeDef::leftAdjust

Select if left adjustment should be done.

Definition at line 906 of file em_adc.h .

Referenced by ADC_InitScan() .

bool ADC_InitScan_TypeDef::prsEnable

Peripheral reflex system trigger enable.

Definition at line 903 of file em_adc.h .

Referenced by ADC_InitScan() , and MIC_init() .

ADC_PRSSEL_TypeDef ADC_InitScan_TypeDef::prsSel

Peripheral reflex system trigger selection. Only applicable if prsEnable is enabled.

Definition at line 867 of file em_adc.h .

Referenced by ADC_InitScan() , and MIC_init() .

ADC_Ref_TypeDef ADC_InitScan_TypeDef::reference

Sample reference selection. Notice that for external references, the ADC calibration register must be set explicitly.

Definition at line 876 of file em_adc.h .

Referenced by ADC_InitScan() , and MIC_init() .

bool ADC_InitScan_TypeDef::rep

Select if continuous conversion until explicit stop.

Definition at line 909 of file em_adc.h .

Referenced by ADC_InitScan() .

ADC_Res_TypeDef ADC_InitScan_TypeDef::resolution

Sample resolution.

Definition at line 879 of file em_adc.h .

Referenced by ADC_InitScan() .


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/emlib/inc/ em_adc.h