VCMP_Init_TypeDef Struct ReferenceEMLIB > VCMP

VCMP Initialization structure

Definition at line 94 of file em_vcmp.h .

#include < em_vcmp.h >

Data Fields

int biasProg
bool enable
bool halfBias
VCMP_Hysteresis_TypeDef hyst
int inactive
bool irqFalling
bool irqRising
bool lowPowerRef
int triggerLevel
VCMP_WarmTime_TypeDef warmup

Field Documentation

int VCMP_Init_TypeDef::biasProg

BIAS current configuration, depends on halfBias setting, above, see reference manual

Definition at line 99 of file em_vcmp.h .

Referenced by VCMP_Init() .

bool VCMP_Init_TypeDef::enable

Enable VCMP after configuration

Definition at line 116 of file em_vcmp.h .

Referenced by VCMP_Init() , and VDDCHECK_LowVoltage() .

bool VCMP_Init_TypeDef::halfBias

If set to true, will reduce by half the bias current

Definition at line 96 of file em_vcmp.h .

Referenced by VCMP_Init() .

VCMP_Hysteresis_TypeDef VCMP_Init_TypeDef::hyst

Hysteresis configuration

Definition at line 107 of file em_vcmp.h .

Referenced by VCMP_Init() .

int VCMP_Init_TypeDef::inactive

Output value when comparator is inactive, should be 0 or 1

Definition at line 109 of file em_vcmp.h .

Referenced by VCMP_Init() .

bool VCMP_Init_TypeDef::irqFalling

Enable interrupt for falling edge

Definition at line 101 of file em_vcmp.h .

Referenced by VCMP_Init() .

bool VCMP_Init_TypeDef::irqRising

Enable interrupt for rising edge

Definition at line 103 of file em_vcmp.h .

Referenced by VCMP_Init() .

bool VCMP_Init_TypeDef::lowPowerRef

Enable low power mode for VDD and bandgap reference

Definition at line 111 of file em_vcmp.h .

Referenced by VCMP_Init() , and VDDCHECK_LowVoltage() .

int VCMP_Init_TypeDef::triggerLevel

Trigger level, according to formula VDD Trigger Level = 1.667V + 0.034V x triggerLevel

Definition at line 114 of file em_vcmp.h .

Referenced by VCMP_Init() , and VDDCHECK_LowVoltage() .

VCMP_WarmTime_TypeDef VCMP_Init_TypeDef::warmup

Warm-up time in clock cycles

Definition at line 105 of file em_vcmp.h .

Referenced by VCMP_Init() , and VDDCHECK_LowVoltage() .


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/emlib/inc/ em_vcmp.h